InspectionAlignmentAssistantBuilderAlignType Enumeration¶
NXOpen.CAM.InspectionAlignmentAssistantBuilder.AlignType is an alias for NXOpen.CAM.InspectionAlignmentAssistantBuilderAlignType
-
class
NXOpen.CAM.
InspectionAlignmentAssistantBuilderAlignType
¶ Bases:
object
Alignment type
Enum Members
Enum Member Enum Member Description PlanePlanePlane Plane, Plane, Plane alignment typePlaneLinePoint Plane, Line, Point alignment typePlaneCylinderCylinder Plane, Cylinder, Cylinder alignment typePlaneBoltHoleCircle Plane, Bolt Hole Circle alignment typeCylinderPlanePlane Cylinder, Plane, Plane alignment typeCylinderPlanePoint Cylinder, Plane, Point alignment typeCylinderPlaneCylinder Cylinder, Plane, Cylinder alignment typeSixPointNest Six Point Nest alignment typeSPFTolerance SPF Tolerance alignment typeRps RPS alignment type-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-