DmCurveBuilder Class¶
-
class
NXOpen.CAM.
DmCurveBuilder
¶ Bases:
NXOpen.TaggedObject
Represents a Curve Drive Method Builder
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
DpmcvDriveCurves | Returns the Drive Curves |
DpmcvEndPercBuilder | Returns the Curve Drive Method End Cut Range builder(inheritable double) |
DpmcvNumSegsBuilder | Returns the Point Type of Curve Drive Method Cut Step Type builder(inheritable int) |
DpmcvStartPercBuilder | Returns the Curve Drive Method Start Cut Range builder(inheritable double) |
DpmcvStepTolBuilder | Returns the Not Point Type of Curve Drive Method Cut Step Type builder(inheritable double) |
DpmcvStepType | Returns or sets the Curve Cut Step Option |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
CreateDpmcvDriveCurve | Create a Drive Curve @return the Drive Curve |
Enumerations¶
DmCurveBuilderDpmcvStepTypes Enumeration | Available types for Cure Drive Cut Step |
Property Detail¶
DpmcvDriveCurves¶
-
DmCurveBuilder.
DpmcvDriveCurves
¶ Returns the Drive Curves
-------------------------------------
Getter Method
Signature
DpmcvDriveCurves()
Returns: the Drive Curves Return type: NXOpen.CAM.DriveChainItemBuilderList
New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
DpmcvEndPercBuilder¶
-
DmCurveBuilder.
DpmcvEndPercBuilder
¶ Returns the Curve Drive Method End Cut Range builder(inheritable double)
-------------------------------------
Getter Method
Signature
DpmcvEndPercBuilder()
Returns: the End Cut Range value Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX5.0.0.
License requirements: None.
DpmcvNumSegsBuilder¶
-
DmCurveBuilder.
DpmcvNumSegsBuilder
¶ Returns the Point Type of Curve Drive Method Cut Step Type builder(inheritable int)
-------------------------------------
Getter Method
Signature
DpmcvNumSegsBuilder()
Returns: the Point Type value Return type: NXOpen.CAM.InheritableIntBuilder
New in version NX5.0.0.
License requirements: None.
DpmcvStartPercBuilder¶
-
DmCurveBuilder.
DpmcvStartPercBuilder
¶ Returns the Curve Drive Method Start Cut Range builder(inheritable double)
-------------------------------------
Getter Method
Signature
DpmcvStartPercBuilder()
Returns: the Start Cut Range value Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX5.0.0.
License requirements: None.
DpmcvStepTolBuilder¶
-
DmCurveBuilder.
DpmcvStepTolBuilder
¶ Returns the Not Point Type of Curve Drive Method Cut Step Type builder(inheritable double)
-------------------------------------
Getter Method
Signature
DpmcvStepTolBuilder()
Returns: not the Point Type value Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX5.0.0.
License requirements: None.
DpmcvStepType¶
-
DmCurveBuilder.
DpmcvStepType
¶ Returns or sets the Curve Cut Step Option
-------------------------------------
Getter Method
Signature
DpmcvStepType()
Returns: the Curve Cut Step Option value Return type: NXOpen.CAM.DmCurveBuilderDpmcvStepTypes
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DpmcvStepType(curveCutStep)
Parameters: curveCutStep ( NXOpen.CAM.DmCurveBuilderDpmcvStepTypes
) – the Curve Cut Step Option valueNew in version NX5.0.0.
License requirements: None.
Method Detail¶
CreateDpmcvDriveCurve¶
-
DmCurveBuilder.
CreateDpmcvDriveCurve
¶ Create a Drive Curve
Signature
CreateDpmcvDriveCurve(section)
Parameters: section ( NXOpen.Section
) –Returns: the Drive Curve Return type: NXOpen.CAM.DriveChainItemBuilder
New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)