DriveChainItemBuilder Class¶
-
class
NXOpen.CAM.
DriveChainItemBuilder
¶ Bases:
NXOpen.Builder
Represents the Drive Chain Item Builder
This cannot be instantiated
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
CurveItem | Returns or sets the curve item |
FeedCutBuilder | Returns or sets the feed rate builder |
FeedrateFlag | Returns or sets the feed rate flag |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
CurveItem¶
-
DriveChainItemBuilder.
CurveItem
¶ Returns or sets the curve item
-------------------------------------
Getter Method
Signature
CurveItem()
Returns: the current value Return type: NXOpen.Section
New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
CurveItem(section)
Parameters: section ( NXOpen.Section
) – the new valueNew in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
FeedCutBuilder¶
-
DriveChainItemBuilder.
FeedCutBuilder
¶ Returns or sets the feed rate builder
-------------------------------------
Getter Method
Signature
FeedCutBuilder()
Returns: the current value Return type: NXOpen.CAM.InheritableFeedBuilder
New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
FeedCutBuilder(feedBuilder)
Parameters: feedBuilder ( NXOpen.CAM.InheritableFeedBuilder
) – the current valueNew in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
FeedrateFlag¶
-
DriveChainItemBuilder.
FeedrateFlag
¶ Returns or sets the feed rate flag
-------------------------------------
Getter Method
Signature
FeedrateFlag()
Returns: the toggle value of Custom Cut Feed Rate Return type: bool New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
FeedrateFlag(flag)
Parameters: flag (bool) – the toggle value of Custom Cut Feed Rate New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
Method Detail¶
Validate¶
-
DriveChainItemBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.