InheritableFeedBuilder Class¶
-
class
NXOpen.CAM.
InheritableFeedBuilder
¶ Bases:
NXOpen.CAM.InheritableBuilder
Represents a builder for an inheritable feed value in of a CAM.
CAMObject .. versionadded:: NX5.0.0
Properties¶
Property | Description |
---|---|
InheritanceStatus | Returns or sets the inheritance status |
Tag | Returns the Tag for this object. |
Unit | Returns or sets the current value |
Value | Returns or sets the current value |
Methods¶
Property Detail¶
Unit¶
-
InheritableFeedBuilder.
Unit
¶ Returns or sets the current value
-------------------------------------
Getter Method
Signature
Unit()
Returns: the current unit Return type: NXOpen.CAM.FeedRateUnit
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Unit(unit)
Parameters: unit ( NXOpen.CAM.FeedRateUnit
) – the new unitNew in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
Value¶
-
InheritableFeedBuilder.
Value
¶ Returns or sets the current value
-------------------------------------
Getter Method
Signature
Value()
Returns: the current value Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Value(inputValue)
Parameters: inputValue (float) – the new value New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)