DmCurveBuilderDpmcvStepTypes Enumeration

NXOpen.CAM.DmCurveBuilder.DpmcvStepTypes is an alias for NXOpen.CAM.DmCurveBuilderDpmcvStepTypes

class NXOpen.CAM.DmCurveBuilderDpmcvStepTypes

Bases: object

Available types for Cure Drive Cut Step

Enum Members

Enum Member Enum Member Description
Tolerance
Tolerance
Number
Number
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.