SearchCriteriaFeatureControlFrameBuilder Class

class NXOpen.Annotations.SearchCriteriaFeatureControlFrameBuilder

Bases: NXOpen.Builder

Represents SearchCriteriaFeatureControlFrameBuilder

To create a new instance of this class, use NXOpen.Annotations.SearchModelViewCollection.CreateSearchCriteriaFeatureControlFrameBuilder()

New in version NX7.5.0.

Properties

Property Description
ByCharacteristic Returns or sets the characteristic toggle
ByCircleU Returns or sets the circle utoggle
ByCircleUValue Returns or sets the circle uvalue toggle
ByFreeState Returns or sets the free state toggle
ByMaximum Returns or sets the maximum toggle
ByPrimaryDatum Returns or sets the primary datum toggle.
ByPrimaryDatumDual Returns or sets the primary datum dual toggle.
ByPrimaryDatumDualMCM Returns or sets the primary datum dual mcmtoggle.
ByPrimaryDatumMCM Returns or sets the primary datum mcmtoggle.
ByProjected Returns or sets the projected toggle
ByProjectedValue Returns or sets the projected value toggle
BySecondaryDatum Returns or sets the secondary datum toggle.
BySecondaryDatumDual Returns or sets the secondary datum dual toggle.
BySecondaryDatumDualMCM Returns or sets the secondary datum dual mcmtoggle.
BySecondaryDatumMCM Returns or sets the secondary datum mcmtoggle.
ByStatistical Returns or sets the statistical toggle
ByTangentPlane Returns or sets the tangent plane toggle
ByTertiaryDatum Returns or sets the tertiary datum toggle.
ByTertiaryDatumDual Returns or sets the tertiary datum dual toggle.
ByTertiaryDatumDualMCM Returns or sets the tertiary datum dual mcmtoggle.
ByTertiaryDatumMCM Returns or sets the tertiary datum mcmtoggle.
ByTolerance Returns or sets the tolerance toggle
ByToleranceMCM Returns or sets the tolerance mcmtoggle
ByZoneShape Returns or sets the zone shape toggle
CharacteristicType Returns or sets the characteristic enum
CircleUType Returns or sets the circle uenum
CircleUValue Returns or sets the circle uvalue
CircleUValueType Returns or sets the circle uvalue enum
DatumExtendedText Returns or sets the datum extended text
DatumExtendedTextToggle Returns or sets the datum extended text toggle
DatumExtendedTextType Returns or sets the datum extended text toggle
DatumMCMToggle Returns or sets the datum mcm toggle
DatumMCMType Returns or sets the datum mcm enum
DatumText Returns or sets the datum text
DatumToggle Returns or sets the datum toggle
FrameStyleType Returns or sets the frame style enum
FreeStateType Returns or sets the free state enum
MaximumText Returns or sets the maximum value
MaximumTextType Returns or sets the maximum text enum
PrimaryDatumDualMCMType Returns or sets the primary datum dual mcmenum.
PrimaryDatumDualText Returns or sets the primary datum dual text.
PrimaryDatumMCMType Returns or sets the primary datum mcmenum.
PrimaryDatumText Returns or sets the primary datum text This property is deprecated.
ProjectedType Returns or sets the projected enum
ProjectedValue Returns or sets the projected value
ProjectedValueType Returns or sets the projected value enum
SecondaryDatumDualMCMType Returns or sets the secondary datum dual mcmenum.
SecondaryDatumDualText Returns or sets the secondary datum dual text.
SecondaryDatumMCMType Returns or sets the secondary datum mcmenum.
SecondaryDatumText Returns or sets the secondary datum text.
StatisticalType Returns or sets the statistical enum
Tag Returns the Tag for this object.
TangentPlaneType Returns or sets the tangent plane enum
TertiaryDatumDualMCMType Returns or sets the tertiary datum dual mcmenum.
TertiaryDatumDualText Returns or sets the tertiary datum dual text.
TertiaryDatumMCMType Returns or sets the tertiary datum mcmenum.
TertiaryDatumText Returns or sets the tertiary datum text.
ToleranceMCMType Returns or sets the tolerance mcmenum
ToleranceText Returns or sets the tolerance text
ToleranceTextType Returns or sets the tolerance text enum
ZoneShapeType Returns or sets the zone shape enum

Methods

Method Description
Commit Commits any edits that have been applied to the builder.
Destroy Deletes the builder, and cleans up any objects created by the builder.
GetCommittedObjects For builders that create more than one object, this method returns the objects that are created by commit.
GetObject Returns the object currently being edited by this builder.
ShowResults Updates the model to reflect the result of an edit to the model for all builders that support showing results.
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Enumerations

SearchCriteriaFeatureControlFrameBuilderCharacteristicOptions Enumeration Lists the search pmi feature control frame type
SearchCriteriaFeatureControlFrameBuilderCircleUOptions Enumeration Lists the status of pmi feature control frame circleU
SearchCriteriaFeatureControlFrameBuilderFrameStyleOptions Enumeration Lists the search pmi feature control frame style
SearchCriteriaFeatureControlFrameBuilderFreeStateOptions Enumeration Lists the status of pmi feature control frame free state
SearchCriteriaFeatureControlFrameBuilderPrimaryDatumDualMCMOptions Enumeration Lists the type of pmi feature control frame primary datum dual MCM
SearchCriteriaFeatureControlFrameBuilderPrimaryDatumMCMOptions Enumeration Lists the type of pmi feature control frame primary datum MCM
SearchCriteriaFeatureControlFrameBuilderProjectedOptions Enumeration Lists the status of pmi feature control frame projected
SearchCriteriaFeatureControlFrameBuilderSecondaryDatumDualMCMOptions Enumeration Lists the type of pmi feature control frame secondary datum dual MCM
SearchCriteriaFeatureControlFrameBuilderSecondaryDatumMCMOptions Enumeration Lists the type of pmi feature control frame secondary datum MCM
SearchCriteriaFeatureControlFrameBuilderStatisticalOptions Enumeration Lists the status of pmi feature control frame statistical
SearchCriteriaFeatureControlFrameBuilderTangentPlaneOptions Enumeration Lists the status of pmi feature control frame tangent plane
SearchCriteriaFeatureControlFrameBuilderTertiaryDatumDualMCMOptions Enumeration Lists the type of pmi feature control frame tertiary datum dual MCM
SearchCriteriaFeatureControlFrameBuilderTertiaryDatumMCMOptions Enumeration Lists the type of pmi feature control frame tertiary datum MCM
SearchCriteriaFeatureControlFrameBuilderToleranceMCMOptions Enumeration Lists the type of pmi feature control frame tolerance MCM
SearchCriteriaFeatureControlFrameBuilderZoneShapeOptions Enumeration Lists the type of pmi feature control frame zone shape

Property Detail

ByCharacteristic

SearchCriteriaFeatureControlFrameBuilder.ByCharacteristic

Returns or sets the characteristic toggle

-------------------------------------

Getter Method

Signature ByCharacteristic()

Returns:
Return type:bool

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ByCharacteristic(characteristic)

Parameters:characteristic (bool) –

New in version NX7.5.0.

License requirements: None.

ByCircleU

SearchCriteriaFeatureControlFrameBuilder.ByCircleU

Returns or sets the circle utoggle

-------------------------------------

Getter Method

Signature ByCircleU()

Returns:
Return type:bool

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ByCircleU(circleU)

Parameters:circleU (bool) –

New in version NX7.5.0.

License requirements: None.

ByCircleUValue

SearchCriteriaFeatureControlFrameBuilder.ByCircleUValue

Returns or sets the circle uvalue toggle

-------------------------------------

Getter Method

Signature ByCircleUValue()

Returns:
Return type:bool

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ByCircleUValue(circleUValue)

Parameters:circleUValue (bool) –

New in version NX7.5.0.

License requirements: None.

ByFreeState

SearchCriteriaFeatureControlFrameBuilder.ByFreeState

Returns or sets the free state toggle

-------------------------------------

Getter Method

Signature ByFreeState()

Returns:
Return type:bool

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ByFreeState(freeState)

Parameters:freeState (bool) –

New in version NX7.5.0.

License requirements: None.

ByMaximum

SearchCriteriaFeatureControlFrameBuilder.ByMaximum

Returns or sets the maximum toggle

-------------------------------------

Getter Method

Signature ByMaximum()

Returns:
Return type:bool

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ByMaximum(maximum)

Parameters:maximum (bool) –

New in version NX7.5.0.

License requirements: None.

ByPrimaryDatum

SearchCriteriaFeatureControlFrameBuilder.ByPrimaryDatum

Returns or sets the primary datum toggle.

This property is deprecated.

-------------------------------------

Getter Method

Signature ByPrimaryDatum()

Returns:
Return type:bool

New in version NX7.5.0.

Deprecated since version NX10.0.0: Use Annotations.SearchCriteriaFeatureControlFrameBuilder.DatumToggle`() instead.

License requirements: None.

-------------------------------------

Setter Method

Signature ByPrimaryDatum(primaryDatum)

Parameters:primaryDatum (bool) –

New in version NX7.5.0.

Deprecated since version NX10.0.0: Use Annotations.SearchCriteriaFeatureControlFrameBuilder.DatumToggle`() instead.

License requirements: None.

ByPrimaryDatumDual

SearchCriteriaFeatureControlFrameBuilder.ByPrimaryDatumDual

Returns or sets the primary datum dual toggle.

This property is deprecated.

-------------------------------------

Getter Method

Signature ByPrimaryDatumDual()

Returns:
Return type:bool

New in version NX7.5.0.

Deprecated since version NX10.0.0: Use Annotations.SearchCriteriaFeatureControlFrameBuilder.DatumToggle`() instead.

License requirements: None.

-------------------------------------

Setter Method

Signature ByPrimaryDatumDual(primaryDatumDual)

Parameters:primaryDatumDual (bool) –

New in version NX7.5.0.

Deprecated since version NX10.0.0: Use Annotations.SearchCriteriaFeatureControlFrameBuilder.DatumToggle`() instead.

License requirements: None.

ByPrimaryDatumDualMCM

SearchCriteriaFeatureControlFrameBuilder.ByPrimaryDatumDualMCM

Returns or sets the primary datum dual mcmtoggle.

This property is deprecated.

-------------------------------------

Getter Method

Signature ByPrimaryDatumDualMCM()

Returns:
Return type:bool

New in version NX7.5.0.

Deprecated since version NX10.0.0: Use Annotations.SearchCriteriaFeatureControlFrameBuilder.DatumMCMToggle`() instead.

License requirements: None.

-------------------------------------

Setter Method

Signature ByPrimaryDatumDualMCM(primaryDatumDualMCM)

Parameters:primaryDatumDualMCM (bool) –

New in version NX7.5.0.

Deprecated since version NX10.0.0: Use Annotations.SearchCriteriaFeatureControlFrameBuilder.DatumMCMToggle`() instead.

License requirements: None.

ByPrimaryDatumMCM

SearchCriteriaFeatureControlFrameBuilder.ByPrimaryDatumMCM

Returns or sets the primary datum mcmtoggle.

This property is deprecated.

-------------------------------------

Getter Method

Signature ByPrimaryDatumMCM()

Returns:
Return type:bool

New in version NX7.5.0.

Deprecated since version NX10.0.0: Use Annotations.SearchCriteriaFeatureControlFrameBuilder.DatumMCMToggle`() instead.

License requirements: None.

-------------------------------------

Setter Method

Signature ByPrimaryDatumMCM(primaryDatumMCM)

Parameters:primaryDatumMCM (bool) –

New in version NX7.5.0.

Deprecated since version NX10.0.0: Use Annotations.SearchCriteriaFeatureControlFrameBuilder.DatumMCMToggle`() instead.

License requirements: None.

ByProjected

SearchCriteriaFeatureControlFrameBuilder.ByProjected

Returns or sets the projected toggle

-------------------------------------

Getter Method

Signature ByProjected()

Returns:
Return type:bool

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ByProjected(projected)

Parameters:projected (bool) –

New in version NX7.5.0.

License requirements: None.

ByProjectedValue

SearchCriteriaFeatureControlFrameBuilder.ByProjectedValue

Returns or sets the projected value toggle

-------------------------------------

Getter Method

Signature ByProjectedValue()

Returns:
Return type:bool

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ByProjectedValue(projectedValue)

Parameters:projectedValue (bool) –

New in version NX7.5.0.

License requirements: None.

BySecondaryDatum

SearchCriteriaFeatureControlFrameBuilder.BySecondaryDatum

Returns or sets the secondary datum toggle.

This property is deprecated.

-------------------------------------

Getter Method

Signature BySecondaryDatum()

Returns:
Return type:bool

New in version NX7.5.0.

Deprecated since version NX10.0.0: Use Annotations.SearchCriteriaFeatureControlFrameBuilder.DatumToggle`() instead.

License requirements: None.

-------------------------------------

Setter Method

Signature BySecondaryDatum(secondaryDatum)

Parameters:secondaryDatum (bool) –

New in version NX7.5.0.

Deprecated since version NX10.0.0: Use Annotations.SearchCriteriaFeatureControlFrameBuilder.DatumToggle`() instead.

License requirements: None.

BySecondaryDatumDual

SearchCriteriaFeatureControlFrameBuilder.BySecondaryDatumDual

Returns or sets the secondary datum dual toggle.

This property is deprecated.

-------------------------------------

Getter Method

Signature BySecondaryDatumDual()

Returns:
Return type:bool

New in version NX7.5.0.

Deprecated since version NX10.0.0: Use Annotations.SearchCriteriaFeatureControlFrameBuilder.DatumToggle`() instead.

License requirements: None.

-------------------------------------

Setter Method

Signature BySecondaryDatumDual(secondaryDatumDual)

Parameters:secondaryDatumDual (bool) –

New in version NX7.5.0.

Deprecated since version NX10.0.0: Use Annotations.SearchCriteriaFeatureControlFrameBuilder.DatumToggle`() instead.

License requirements: None.

BySecondaryDatumDualMCM

SearchCriteriaFeatureControlFrameBuilder.BySecondaryDatumDualMCM

Returns or sets the secondary datum dual mcmtoggle.

This property is deprecated.

-------------------------------------

Getter Method

Signature BySecondaryDatumDualMCM()

Returns:
Return type:bool

New in version NX7.5.0.

Deprecated since version NX10.0.0: Use Annotations.SearchCriteriaFeatureControlFrameBuilder.DatumMCMToggle`() instead.

License requirements: None.

-------------------------------------

Setter Method

Signature BySecondaryDatumDualMCM(secondaryDatumDualMCM)

Parameters:secondaryDatumDualMCM (bool) –

New in version NX7.5.0.

Deprecated since version NX10.0.0: Use Annotations.SearchCriteriaFeatureControlFrameBuilder.DatumMCMToggle`() instead.

License requirements: None.

BySecondaryDatumMCM

SearchCriteriaFeatureControlFrameBuilder.BySecondaryDatumMCM

Returns or sets the secondary datum mcmtoggle.

This property is deprecated.

-------------------------------------

Getter Method

Signature BySecondaryDatumMCM()

Returns:
Return type:bool

New in version NX7.5.0.

Deprecated since version NX10.0.0: Use Annotations.SearchCriteriaFeatureControlFrameBuilder.DatumMCMToggle`() instead.

License requirements: None.

-------------------------------------

Setter Method

Signature BySecondaryDatumMCM(secondaryDatumMCM)

Parameters:secondaryDatumMCM (bool) –

New in version NX7.5.0.

Deprecated since version NX10.0.0: Use Annotations.SearchCriteriaFeatureControlFrameBuilder.DatumMCMToggle`() instead.

License requirements: None.

ByStatistical

SearchCriteriaFeatureControlFrameBuilder.ByStatistical

Returns or sets the statistical toggle

-------------------------------------

Getter Method

Signature ByStatistical()

Returns:
Return type:bool

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ByStatistical(statistical)

Parameters:statistical (bool) –

New in version NX7.5.0.

License requirements: None.

ByTangentPlane

SearchCriteriaFeatureControlFrameBuilder.ByTangentPlane

Returns or sets the tangent plane toggle

-------------------------------------

Getter Method

Signature ByTangentPlane()

Returns:
Return type:bool

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ByTangentPlane(tangentPlane)

Parameters:tangentPlane (bool) –

New in version NX7.5.0.

License requirements: None.

ByTertiaryDatum

SearchCriteriaFeatureControlFrameBuilder.ByTertiaryDatum

Returns or sets the tertiary datum toggle.

This property is deprecated.

-------------------------------------

Getter Method

Signature ByTertiaryDatum()

Returns:
Return type:bool

New in version NX7.5.0.

Deprecated since version NX10.0.0: Use Annotations.SearchCriteriaFeatureControlFrameBuilder.DatumToggle`() instead.

License requirements: None.

-------------------------------------

Setter Method

Signature ByTertiaryDatum(tertiaryDatum)

Parameters:tertiaryDatum (bool) –

New in version NX7.5.0.

Deprecated since version NX10.0.0: Use Annotations.SearchCriteriaFeatureControlFrameBuilder.DatumToggle`() instead.

License requirements: None.

ByTertiaryDatumDual

SearchCriteriaFeatureControlFrameBuilder.ByTertiaryDatumDual

Returns or sets the tertiary datum dual toggle.

This property is deprecated.

-------------------------------------

Getter Method

Signature ByTertiaryDatumDual()

Returns:
Return type:bool

New in version NX7.5.0.

Deprecated since version NX10.0.0: Use Annotations.SearchCriteriaFeatureControlFrameBuilder.DatumToggle`() instead.

License requirements: None.

-------------------------------------

Setter Method

Signature ByTertiaryDatumDual(tertiaryDatumDual)

Parameters:tertiaryDatumDual (bool) –

New in version NX7.5.0.

Deprecated since version NX10.0.0: Use Annotations.SearchCriteriaFeatureControlFrameBuilder.DatumToggle`() instead.

License requirements: None.

ByTertiaryDatumDualMCM

SearchCriteriaFeatureControlFrameBuilder.ByTertiaryDatumDualMCM

Returns or sets the tertiary datum dual mcmtoggle.

This property is deprecated.

-------------------------------------

Getter Method

Signature ByTertiaryDatumDualMCM()

Returns:
Return type:bool

New in version NX7.5.0.

Deprecated since version NX10.0.0: Use Annotations.SearchCriteriaFeatureControlFrameBuilder.DatumMCMToggle`() instead.

License requirements: None.

-------------------------------------

Setter Method

Signature ByTertiaryDatumDualMCM(tertiaryDatumDualMCM)

Parameters:tertiaryDatumDualMCM (bool) –

New in version NX7.5.0.

Deprecated since version NX10.0.0: Use Annotations.SearchCriteriaFeatureControlFrameBuilder.DatumMCMToggle`() instead.

License requirements: None.

ByTertiaryDatumMCM

SearchCriteriaFeatureControlFrameBuilder.ByTertiaryDatumMCM

Returns or sets the tertiary datum mcmtoggle.

This property is deprecated.

-------------------------------------

Getter Method

Signature ByTertiaryDatumMCM()

Returns:
Return type:bool

New in version NX7.5.0.

Deprecated since version NX10.0.0: Use Annotations.SearchCriteriaFeatureControlFrameBuilder.DatumMCMToggle`() instead.

License requirements: None.

-------------------------------------

Setter Method

Signature ByTertiaryDatumMCM(tertiaryDatumMCM)

Parameters:tertiaryDatumMCM (bool) –

New in version NX7.5.0.

Deprecated since version NX10.0.0: Use Annotations.SearchCriteriaFeatureControlFrameBuilder.DatumMCMToggle`() instead.

License requirements: None.

ByTolerance

SearchCriteriaFeatureControlFrameBuilder.ByTolerance

Returns or sets the tolerance toggle

-------------------------------------

Getter Method

Signature ByTolerance()

Returns:
Return type:bool

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ByTolerance(tolerance)

Parameters:tolerance (bool) –

New in version NX7.5.0.

License requirements: None.

ByToleranceMCM

SearchCriteriaFeatureControlFrameBuilder.ByToleranceMCM

Returns or sets the tolerance mcmtoggle

-------------------------------------

Getter Method

Signature ByToleranceMCM()

Returns:
Return type:bool

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ByToleranceMCM(toleranceMCM)

Parameters:toleranceMCM (bool) –

New in version NX7.5.0.

License requirements: None.

ByZoneShape

SearchCriteriaFeatureControlFrameBuilder.ByZoneShape

Returns or sets the zone shape toggle

-------------------------------------

Getter Method

Signature ByZoneShape()

Returns:
Return type:bool

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ByZoneShape(zoneShape)

Parameters:zoneShape (bool) –

New in version NX7.5.0.

License requirements: None.

CharacteristicType

SearchCriteriaFeatureControlFrameBuilder.CharacteristicType

Returns or sets the characteristic enum

-------------------------------------

Getter Method

Signature CharacteristicType()

Returns:
Return type:NXOpen.Annotations.SearchCriteriaFeatureControlFrameBuilderCharacteristicOptions

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature CharacteristicType(characteristicType)

Parameters:characteristicType (NXOpen.Annotations.SearchCriteriaFeatureControlFrameBuilderCharacteristicOptions) –

New in version NX7.5.0.

License requirements: None.

CircleUType

SearchCriteriaFeatureControlFrameBuilder.CircleUType

Returns or sets the circle uenum

-------------------------------------

Getter Method

Signature CircleUType()

Returns:
Return type:NXOpen.Annotations.SearchCriteriaFeatureControlFrameBuilderCircleUOptions

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature CircleUType(circleUType)

Parameters:circleUType (NXOpen.Annotations.SearchCriteriaFeatureControlFrameBuilderCircleUOptions) –

New in version NX7.5.0.

License requirements: None.

CircleUValue

SearchCriteriaFeatureControlFrameBuilder.CircleUValue

Returns or sets the circle uvalue

-------------------------------------

Getter Method

Signature CircleUValue()

Returns:
Return type:float

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature CircleUValue(circleUValue)

Parameters:circleUValue (float) –

New in version NX7.5.0.

License requirements: None.

CircleUValueType

SearchCriteriaFeatureControlFrameBuilder.CircleUValueType

Returns or sets the circle uvalue enum

-------------------------------------

Getter Method

Signature CircleUValueType()

Returns:
Return type:NXOpen.Annotations.SearchModelViewBuilderValueComparisionOptions

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature CircleUValueType(circleUValueType)

Parameters:circleUValueType (NXOpen.Annotations.SearchModelViewBuilderValueComparisionOptions) –

New in version NX7.5.0.

License requirements: None.

DatumExtendedText

SearchCriteriaFeatureControlFrameBuilder.DatumExtendedText

Returns or sets the datum extended text

-------------------------------------

Getter Method

Signature DatumExtendedText()

Returns:
Return type:str

New in version NX10.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature DatumExtendedText(datumExtendedText)

Parameters:datumExtendedText (str) –

New in version NX10.0.0.

License requirements: None.

DatumExtendedTextToggle

SearchCriteriaFeatureControlFrameBuilder.DatumExtendedTextToggle

Returns or sets the datum extended text toggle

-------------------------------------

Getter Method

Signature DatumExtendedTextToggle()

Returns:
Return type:bool

New in version NX10.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature DatumExtendedTextToggle(datumExtendedTextToggle)

Parameters:datumExtendedTextToggle (bool) –

New in version NX10.0.0.

License requirements: None.

DatumExtendedTextType

SearchCriteriaFeatureControlFrameBuilder.DatumExtendedTextType

Returns or sets the datum extended text toggle

-------------------------------------

Getter Method

Signature DatumExtendedTextType()

Returns:
Return type:NXOpen.Annotations.SearchModelViewBuilderTextComparisionOptions

New in version NX10.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature DatumExtendedTextType(datumExtendedTextType)

Parameters:datumExtendedTextType (NXOpen.Annotations.SearchModelViewBuilderTextComparisionOptions) –

New in version NX10.0.0.

License requirements: None.

DatumMCMToggle

SearchCriteriaFeatureControlFrameBuilder.DatumMCMToggle

Returns or sets the datum mcm toggle

-------------------------------------

Getter Method

Signature DatumMCMToggle()

Returns:
Return type:bool

New in version NX10.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature DatumMCMToggle(datumMCM)

Parameters:datumMCM (bool) –

New in version NX10.0.0.

License requirements: None.

DatumMCMType

SearchCriteriaFeatureControlFrameBuilder.DatumMCMType

Returns or sets the datum mcm enum

-------------------------------------

Getter Method

Signature DatumMCMType()

Returns:
Return type:NXOpen.Annotations.SearchCriteriaFeatureControlFrameBuilderPrimaryDatumMCMOptions

New in version NX10.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature DatumMCMType(datumMCMType)

Parameters:datumMCMType (NXOpen.Annotations.SearchCriteriaFeatureControlFrameBuilderPrimaryDatumMCMOptions) –

New in version NX10.0.0.

License requirements: None.

DatumText

SearchCriteriaFeatureControlFrameBuilder.DatumText

Returns or sets the datum text

-------------------------------------

Getter Method

Signature DatumText()

Returns:
Return type:str

New in version NX10.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature DatumText(datumText)

Parameters:datumText (str) –

New in version NX10.0.0.

License requirements: None.

DatumToggle

SearchCriteriaFeatureControlFrameBuilder.DatumToggle

Returns or sets the datum toggle

-------------------------------------

Getter Method

Signature DatumToggle()

Returns:
Return type:bool

New in version NX10.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature DatumToggle(datumToggle)

Parameters:datumToggle (bool) –

New in version NX10.0.0.

License requirements: None.

FrameStyleType

SearchCriteriaFeatureControlFrameBuilder.FrameStyleType

Returns or sets the frame style enum

-------------------------------------

Getter Method

Signature FrameStyleType()

Returns:
Return type:NXOpen.Annotations.SearchCriteriaFeatureControlFrameBuilderFrameStyleOptions

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature FrameStyleType(frameStyleType)

Parameters:frameStyleType (NXOpen.Annotations.SearchCriteriaFeatureControlFrameBuilderFrameStyleOptions) –

New in version NX7.5.0.

License requirements: None.

FreeStateType

SearchCriteriaFeatureControlFrameBuilder.FreeStateType

Returns or sets the free state enum

-------------------------------------

Getter Method

Signature FreeStateType()

Returns:
Return type:NXOpen.Annotations.SearchCriteriaFeatureControlFrameBuilderFreeStateOptions

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature FreeStateType(freeStateType)

Parameters:freeStateType (NXOpen.Annotations.SearchCriteriaFeatureControlFrameBuilderFreeStateOptions) –

New in version NX7.5.0.

License requirements: None.

MaximumText

SearchCriteriaFeatureControlFrameBuilder.MaximumText

Returns or sets the maximum value

-------------------------------------

Getter Method

Signature MaximumText()

Returns:
Return type:str

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature MaximumText(maximumText)

Parameters:maximumText (str) –

New in version NX7.5.0.

License requirements: None.

MaximumTextType

SearchCriteriaFeatureControlFrameBuilder.MaximumTextType

Returns or sets the maximum text enum

-------------------------------------

Getter Method

Signature MaximumTextType()

Returns:
Return type:NXOpen.Annotations.SearchModelViewBuilderTextComparisionOptions

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature MaximumTextType(maximumTextType)

Parameters:maximumTextType (NXOpen.Annotations.SearchModelViewBuilderTextComparisionOptions) –

New in version NX7.5.0.

License requirements: None.

PrimaryDatumDualMCMType

SearchCriteriaFeatureControlFrameBuilder.PrimaryDatumDualMCMType

Returns or sets the primary datum dual mcmenum.

This property is deprecated.

-------------------------------------

Getter Method

Signature PrimaryDatumDualMCMType()

Returns:
Return type:NXOpen.Annotations.SearchCriteriaFeatureControlFrameBuilderPrimaryDatumDualMCMOptions

New in version NX7.5.0.

Deprecated since version NX10.0.0: Use Annotations.SearchCriteriaFeatureControlFrameBuilder.DatumMCMType`() instead.

License requirements: None.

-------------------------------------

Setter Method

Signature PrimaryDatumDualMCMType(primaryDatumDualMCMType)

Parameters:primaryDatumDualMCMType (NXOpen.Annotations.SearchCriteriaFeatureControlFrameBuilderPrimaryDatumDualMCMOptions) –

New in version NX7.5.0.

Deprecated since version NX10.0.0: Use Annotations.SearchCriteriaFeatureControlFrameBuilder.DatumMCMType`() instead.

License requirements: None.

PrimaryDatumDualText

SearchCriteriaFeatureControlFrameBuilder.PrimaryDatumDualText

Returns or sets the primary datum dual text.

This property is deprecated.

-------------------------------------

Getter Method

Signature PrimaryDatumDualText()

Returns:
Return type:str

New in version NX7.5.0.

Deprecated since version NX10.0.0: Use Annotations.SearchCriteriaFeatureControlFrameBuilder.DatumText`() instead.

License requirements: None.

-------------------------------------

Setter Method

Signature PrimaryDatumDualText(primaryDatumDualText)

Parameters:primaryDatumDualText (str) –

New in version NX7.5.0.

Deprecated since version NX10.0.0: Use Annotations.SearchCriteriaFeatureControlFrameBuilder.DatumText`() instead.

License requirements: None.

PrimaryDatumMCMType

SearchCriteriaFeatureControlFrameBuilder.PrimaryDatumMCMType

Returns or sets the primary datum mcmenum.

This property is deprecated.

-------------------------------------

Getter Method

Signature PrimaryDatumMCMType()

Returns:
Return type:NXOpen.Annotations.SearchCriteriaFeatureControlFrameBuilderPrimaryDatumMCMOptions

New in version NX7.5.0.

Deprecated since version NX10.0.0: Use Annotations.SearchCriteriaFeatureControlFrameBuilder.DatumMCMType`() instead.

License requirements: None.

-------------------------------------

Setter Method

Signature PrimaryDatumMCMType(primaryDatumMCMType)

Parameters:primaryDatumMCMType (NXOpen.Annotations.SearchCriteriaFeatureControlFrameBuilderPrimaryDatumMCMOptions) –

New in version NX7.5.0.

Deprecated since version NX10.0.0: Use Annotations.SearchCriteriaFeatureControlFrameBuilder.DatumMCMType`() instead.

License requirements: None.

PrimaryDatumText

SearchCriteriaFeatureControlFrameBuilder.PrimaryDatumText

Returns or sets the primary datum text This property is deprecated.

-------------------------------------

Getter Method

Signature PrimaryDatumText()

Returns:
Return type:str

New in version NX7.5.0.

Deprecated since version NX10.0.0: Use Annotations.SearchCriteriaFeatureControlFrameBuilder.DatumText`() instead.

License requirements: None.

-------------------------------------

Setter Method

Signature PrimaryDatumText(primaryDatumText)

Parameters:primaryDatumText (str) –

New in version NX7.5.0.

Deprecated since version NX10.0.0: Use Annotations.SearchCriteriaFeatureControlFrameBuilder.DatumText`() instead.

License requirements: None.

ProjectedType

SearchCriteriaFeatureControlFrameBuilder.ProjectedType

Returns or sets the projected enum

-------------------------------------

Getter Method

Signature ProjectedType()

Returns:
Return type:NXOpen.Annotations.SearchCriteriaFeatureControlFrameBuilderProjectedOptions

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ProjectedType(projectedType)

Parameters:projectedType (NXOpen.Annotations.SearchCriteriaFeatureControlFrameBuilderProjectedOptions) –

New in version NX7.5.0.

License requirements: None.

ProjectedValue

SearchCriteriaFeatureControlFrameBuilder.ProjectedValue

Returns or sets the projected value

-------------------------------------

Getter Method

Signature ProjectedValue()

Returns:
Return type:float

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ProjectedValue(projectedValue)

Parameters:projectedValue (float) –

New in version NX7.5.0.

License requirements: None.

ProjectedValueType

SearchCriteriaFeatureControlFrameBuilder.ProjectedValueType

Returns or sets the projected value enum

-------------------------------------

Getter Method

Signature ProjectedValueType()

Returns:
Return type:NXOpen.Annotations.SearchModelViewBuilderValueComparisionOptions

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ProjectedValueType(projectedValueType)

Parameters:projectedValueType (NXOpen.Annotations.SearchModelViewBuilderValueComparisionOptions) –

New in version NX7.5.0.

License requirements: None.

SecondaryDatumDualMCMType

SearchCriteriaFeatureControlFrameBuilder.SecondaryDatumDualMCMType

Returns or sets the secondary datum dual mcmenum.

This property is deprecated.

-------------------------------------

Getter Method

Signature SecondaryDatumDualMCMType()

Returns:
Return type:NXOpen.Annotations.SearchCriteriaFeatureControlFrameBuilderSecondaryDatumDualMCMOptions

New in version NX7.5.0.

Deprecated since version NX10.0.0: Use Annotations.SearchCriteriaFeatureControlFrameBuilder.DatumMCMType`() instead.

License requirements: None.

-------------------------------------

Setter Method

Signature SecondaryDatumDualMCMType(secondaryDatumDualMCMType)

Parameters:secondaryDatumDualMCMType (NXOpen.Annotations.SearchCriteriaFeatureControlFrameBuilderSecondaryDatumDualMCMOptions) –

New in version NX7.5.0.

Deprecated since version NX10.0.0: Use Annotations.SearchCriteriaFeatureControlFrameBuilder.DatumMCMType`() instead.

License requirements: None.

SecondaryDatumDualText

SearchCriteriaFeatureControlFrameBuilder.SecondaryDatumDualText

Returns or sets the secondary datum dual text.

This property is deprecated.

-------------------------------------

Getter Method

Signature SecondaryDatumDualText()

Returns:
Return type:str

New in version NX7.5.0.

Deprecated since version NX10.0.0: Use Annotations.SearchCriteriaFeatureControlFrameBuilder.DatumText`() instead.

License requirements: None.

-------------------------------------

Setter Method

Signature SecondaryDatumDualText(secondaryDatumDualText)

Parameters:secondaryDatumDualText (str) –

New in version NX7.5.0.

Deprecated since version NX10.0.0: Use Annotations.SearchCriteriaFeatureControlFrameBuilder.DatumText`() instead.

License requirements: None.

SecondaryDatumMCMType

SearchCriteriaFeatureControlFrameBuilder.SecondaryDatumMCMType

Returns or sets the secondary datum mcmenum.

This property is deprecated.

-------------------------------------

Getter Method

Signature SecondaryDatumMCMType()

Returns:
Return type:NXOpen.Annotations.SearchCriteriaFeatureControlFrameBuilderSecondaryDatumMCMOptions

New in version NX7.5.0.

Deprecated since version NX10.0.0: Use Annotations.SearchCriteriaFeatureControlFrameBuilder.DatumMCMType`() instead.

License requirements: None.

-------------------------------------

Setter Method

Signature SecondaryDatumMCMType(secondaryDatumMCMType)

Parameters:secondaryDatumMCMType (NXOpen.Annotations.SearchCriteriaFeatureControlFrameBuilderSecondaryDatumMCMOptions) –

New in version NX7.5.0.

Deprecated since version NX10.0.0: Use Annotations.SearchCriteriaFeatureControlFrameBuilder.DatumMCMType`() instead.

License requirements: None.

SecondaryDatumText

SearchCriteriaFeatureControlFrameBuilder.SecondaryDatumText

Returns or sets the secondary datum text.

This property is deprecated.

-------------------------------------

Getter Method

Signature SecondaryDatumText()

Returns:
Return type:str

New in version NX7.5.0.

Deprecated since version NX10.0.0: Use Annotations.SearchCriteriaFeatureControlFrameBuilder.DatumText`() instead.

License requirements: None.

-------------------------------------

Setter Method

Signature SecondaryDatumText(secondaryDatumText)

Parameters:secondaryDatumText (str) –

New in version NX7.5.0.

Deprecated since version NX10.0.0: Use Annotations.SearchCriteriaFeatureControlFrameBuilder.DatumText`() instead.

License requirements: None.

StatisticalType

SearchCriteriaFeatureControlFrameBuilder.StatisticalType

Returns or sets the statistical enum

-------------------------------------

Getter Method

Signature StatisticalType()

Returns:
Return type:NXOpen.Annotations.SearchCriteriaFeatureControlFrameBuilderStatisticalOptions

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature StatisticalType(statisticalType)

Parameters:statisticalType (NXOpen.Annotations.SearchCriteriaFeatureControlFrameBuilderStatisticalOptions) –

New in version NX7.5.0.

License requirements: None.

TangentPlaneType

SearchCriteriaFeatureControlFrameBuilder.TangentPlaneType

Returns or sets the tangent plane enum

-------------------------------------

Getter Method

Signature TangentPlaneType()

Returns:
Return type:NXOpen.Annotations.SearchCriteriaFeatureControlFrameBuilderTangentPlaneOptions

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature TangentPlaneType(tangentPlaneType)

Parameters:tangentPlaneType (NXOpen.Annotations.SearchCriteriaFeatureControlFrameBuilderTangentPlaneOptions) –

New in version NX7.5.0.

License requirements: None.

TertiaryDatumDualMCMType

SearchCriteriaFeatureControlFrameBuilder.TertiaryDatumDualMCMType

Returns or sets the tertiary datum dual mcmenum.

This property is deprecated.

-------------------------------------

Getter Method

Signature TertiaryDatumDualMCMType()

Returns:
Return type:NXOpen.Annotations.SearchCriteriaFeatureControlFrameBuilderTertiaryDatumDualMCMOptions

New in version NX7.5.0.

Deprecated since version NX10.0.0: Use Annotations.SearchCriteriaFeatureControlFrameBuilder.DatumMCMType`() instead.

License requirements: None.

-------------------------------------

Setter Method

Signature TertiaryDatumDualMCMType(tertiaryDatumDualMCMType)

Parameters:tertiaryDatumDualMCMType (NXOpen.Annotations.SearchCriteriaFeatureControlFrameBuilderTertiaryDatumDualMCMOptions) –

New in version NX7.5.0.

Deprecated since version NX10.0.0: Use Annotations.SearchCriteriaFeatureControlFrameBuilder.DatumMCMType`() instead.

License requirements: None.

TertiaryDatumDualText

SearchCriteriaFeatureControlFrameBuilder.TertiaryDatumDualText

Returns or sets the tertiary datum dual text.

This property is deprecated.

-------------------------------------

Getter Method

Signature TertiaryDatumDualText()

Returns:
Return type:str

New in version NX7.5.0.

Deprecated since version NX10.0.0: Use Annotations.SearchCriteriaFeatureControlFrameBuilder.DatumText`() instead.

License requirements: None.

-------------------------------------

Setter Method

Signature TertiaryDatumDualText(tertiaryDatumDualText)

Parameters:tertiaryDatumDualText (str) –

New in version NX7.5.0.

Deprecated since version NX10.0.0: Use Annotations.SearchCriteriaFeatureControlFrameBuilder.DatumText`() instead.

License requirements: None.

TertiaryDatumMCMType

SearchCriteriaFeatureControlFrameBuilder.TertiaryDatumMCMType

Returns or sets the tertiary datum mcmenum.

This property is deprecated.

-------------------------------------

Getter Method

Signature TertiaryDatumMCMType()

Returns:
Return type:NXOpen.Annotations.SearchCriteriaFeatureControlFrameBuilderTertiaryDatumMCMOptions

New in version NX7.5.0.

Deprecated since version NX10.0.0: Use Annotations.SearchCriteriaFeatureControlFrameBuilder.DatumMCMType`() instead.

License requirements: None.

-------------------------------------

Setter Method

Signature TertiaryDatumMCMType(tertiaryDatumMCMType)

Parameters:tertiaryDatumMCMType (NXOpen.Annotations.SearchCriteriaFeatureControlFrameBuilderTertiaryDatumMCMOptions) –

New in version NX7.5.0.

Deprecated since version NX10.0.0: Use Annotations.SearchCriteriaFeatureControlFrameBuilder.DatumMCMType`() instead.

License requirements: None.

TertiaryDatumText

SearchCriteriaFeatureControlFrameBuilder.TertiaryDatumText

Returns or sets the tertiary datum text.

This property is deprecated.

-------------------------------------

Getter Method

Signature TertiaryDatumText()

Returns:
Return type:str

New in version NX7.5.0.

Deprecated since version NX10.0.0: Use Annotations.SearchCriteriaFeatureControlFrameBuilder.DatumText`() instead.

License requirements: None.

-------------------------------------

Setter Method

Signature TertiaryDatumText(tertiaryDatumText)

Parameters:tertiaryDatumText (str) –

New in version NX7.5.0.

Deprecated since version NX10.0.0: Use Annotations.SearchCriteriaFeatureControlFrameBuilder.DatumText`() instead.

License requirements: None.

ToleranceMCMType

SearchCriteriaFeatureControlFrameBuilder.ToleranceMCMType

Returns or sets the tolerance mcmenum

-------------------------------------

Getter Method

Signature ToleranceMCMType()

Returns:
Return type:NXOpen.Annotations.SearchCriteriaFeatureControlFrameBuilderToleranceMCMOptions

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ToleranceMCMType(toleranceMCMType)

Parameters:toleranceMCMType (NXOpen.Annotations.SearchCriteriaFeatureControlFrameBuilderToleranceMCMOptions) –

New in version NX7.5.0.

License requirements: None.

ToleranceText

SearchCriteriaFeatureControlFrameBuilder.ToleranceText

Returns or sets the tolerance text

-------------------------------------

Getter Method

Signature ToleranceText()

Returns:
Return type:str

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ToleranceText(toleranceText)

Parameters:toleranceText (str) –

New in version NX7.5.0.

License requirements: None.

ToleranceTextType

SearchCriteriaFeatureControlFrameBuilder.ToleranceTextType

Returns or sets the tolerance text enum

-------------------------------------

Getter Method

Signature ToleranceTextType()

Returns:
Return type:NXOpen.Annotations.SearchModelViewBuilderTextComparisionOptions

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ToleranceTextType(toleranceTextType)

Parameters:toleranceTextType (NXOpen.Annotations.SearchModelViewBuilderTextComparisionOptions) –

New in version NX7.5.0.

License requirements: None.

ZoneShapeType

SearchCriteriaFeatureControlFrameBuilder.ZoneShapeType

Returns or sets the zone shape enum

-------------------------------------

Getter Method

Signature ZoneShapeType()

Returns:
Return type:NXOpen.Annotations.SearchCriteriaFeatureControlFrameBuilderZoneShapeOptions

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ZoneShapeType(zoneShapeType)

Parameters:zoneShapeType (NXOpen.Annotations.SearchCriteriaFeatureControlFrameBuilderZoneShapeOptions) –

New in version NX7.5.0.

License requirements: None.

Method Detail

Validate

SearchCriteriaFeatureControlFrameBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.