SearchCriteriaFeatureControlFrameBuilderFreeStateOptions Enumeration

NXOpen.Annotations.SearchCriteriaFeatureControlFrameBuilder.FreeStateOptions is an alias for NXOpen.Annotations.SearchCriteriaFeatureControlFrameBuilderFreeStateOptions

class NXOpen.Annotations.SearchCriteriaFeatureControlFrameBuilderFreeStateOptions

Bases: object

Lists the status of pmi feature control frame free state

Enum Members

Enum Member Enum Member Description
Yes
have free state
No
have no free state
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.