SearchCriteriaFeatureControlFrameBuilderTangentPlaneOptions Enumeration

NXOpen.Annotations.SearchCriteriaFeatureControlFrameBuilder.TangentPlaneOptions is an alias for NXOpen.Annotations.SearchCriteriaFeatureControlFrameBuilderTangentPlaneOptions

class NXOpen.Annotations.SearchCriteriaFeatureControlFrameBuilderTangentPlaneOptions

Bases: object

Lists the status of pmi feature control frame tangent plane

Enum Members

Enum Member Enum Member Description
Yes
have tangent plane
No
have no tangent plane
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.