SearchCriteriaFeatureControlFrameBuilderStatisticalOptions Enumeration

NXOpen.Annotations.SearchCriteriaFeatureControlFrameBuilder.StatisticalOptions is an alias for NXOpen.Annotations.SearchCriteriaFeatureControlFrameBuilderStatisticalOptions

class NXOpen.Annotations.SearchCriteriaFeatureControlFrameBuilderStatisticalOptions

Bases: object

Lists the status of pmi feature control frame statistical

Enum Members

Enum Member Enum Member Description
Yes
have statistical
No
have no statistical
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.