RadialStyleBuilder Class¶
-
class
NXOpen.Annotations.
RadialStyleBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.Annotations.RadialStyleBuilder
.This class queries and sets preferences specific to radial dimensions when creating or editing a radial type dimension.
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
DiameterRadiusPlacement | Returns or sets the diameter radius symbol placement with respect to the dimension text. |
DiameterSymbol | Returns or sets the text for a user-defined diameter symbol |
DiameterSymbolType | Returns or sets the diameter symbol type |
FoldedRadiusAngle | Returns or sets the folded radius angle |
RadiusSymbol | Returns or sets the text for a user-defined radius symbol |
RadiusSymbolType | Returns or sets the radius symbol type |
SymbolToDimensionTextDistance | Returns or sets the symbol to dimension text distance in character spaces |
Tag | Returns the Tag for this object. |
TextAboveLeader | Returns or sets the location of the dimension text relative to the leader stub |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
DiameterRadiusPlacement¶
-
RadialStyleBuilder.
DiameterRadiusPlacement
¶ Returns or sets the diameter radius symbol placement with respect to the dimension text.
One of the options specifies that no symbol be displayed
-------------------------------------
Getter Method
Signature
DiameterRadiusPlacement()
Returns: Return type: NXOpen.Annotations.DiameterRadiusSymbolPlacement
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DiameterRadiusPlacement(diameterRadiusPlacement)
Parameters: diameterRadiusPlacement ( NXOpen.Annotations.DiameterRadiusSymbolPlacement
) –New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
DiameterSymbol¶
-
RadialStyleBuilder.
DiameterSymbol
¶ Returns or sets the text for a user-defined diameter symbol
-------------------------------------
Getter Method
Signature
DiameterSymbol()
Returns: Return type: str New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DiameterSymbol(diameterSymbol)
Parameters: diameterSymbol (str) – New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
DiameterSymbolType¶
-
RadialStyleBuilder.
DiameterSymbolType
¶ Returns or sets the diameter symbol type
-------------------------------------
Getter Method
Signature
DiameterSymbolType()
Returns: Return type: NXOpen.Annotations.DiameterSymbol
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DiameterSymbolType(diameterSymbolType)
Parameters: diameterSymbolType ( NXOpen.Annotations.DiameterSymbol
) –New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
FoldedRadiusAngle¶
-
RadialStyleBuilder.
FoldedRadiusAngle
¶ Returns or sets the folded radius angle
-------------------------------------
Getter Method
Signature
FoldedRadiusAngle()
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FoldedRadiusAngle(foldedRadiusAngle)
Parameters: foldedRadiusAngle (float) – New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
RadiusSymbol¶
-
RadialStyleBuilder.
RadiusSymbol
¶ Returns or sets the text for a user-defined radius symbol
-------------------------------------
Getter Method
Signature
RadiusSymbol()
Returns: Return type: str New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RadiusSymbol(radiusSymbol)
Parameters: radiusSymbol (str) – New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
RadiusSymbolType¶
-
RadialStyleBuilder.
RadiusSymbolType
¶ Returns or sets the radius symbol type
-------------------------------------
Getter Method
Signature
RadiusSymbolType()
Returns: Return type: NXOpen.Annotations.RadiusSymbol
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RadiusSymbolType(radiusSymbolType)
Parameters: radiusSymbolType ( NXOpen.Annotations.RadiusSymbol
) –New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
SymbolToDimensionTextDistance¶
-
RadialStyleBuilder.
SymbolToDimensionTextDistance
¶ Returns or sets the symbol to dimension text distance in character spaces
-------------------------------------
Getter Method
Signature
SymbolToDimensionTextDistance()
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SymbolToDimensionTextDistance(symbolToDimensionTextDistance)
Parameters: symbolToDimensionTextDistance (float) – New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
TextAboveLeader¶
-
RadialStyleBuilder.
TextAboveLeader
¶ Returns or sets the location of the dimension text relative to the leader stub
-------------------------------------
Getter Method
Signature
TextAboveLeader()
Returns: Return type: NXOpen.Annotations.DiameterRadiusLeaderStub
New in version NX6.0.0.
Deprecated since version NX9.0.0: Use
NXOpen.Annotations.DimensionStyleBuilder.TextPosition()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
TextAboveLeader(textAboveLeader)
Parameters: textAboveLeader ( NXOpen.Annotations.DiameterRadiusLeaderStub
) –New in version NX6.0.0.
Deprecated since version NX9.0.0: Use
NXOpen.Annotations.DimensionStyleBuilder.TextPosition()
instead.License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
Method Detail¶
Validate¶
-
RadialStyleBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.