DiameterRadiusSymbolPlacement Enumeration¶
-
class
NXOpen.Annotations.
DiameterRadiusSymbolPlacement
¶ Bases:
object
Specifies the diameter/radius symbol placement relative to the dimension text Enum Members
Enum Member Enum Member Description Below Specifies diameter/radius symbol is placed below dimension textAbove Specifies diameter/radius symbol is placed above dimension textAfter Specifies diameter/radius symbol is placed after dimension textBefore Specifies diameter/radius symbol is placed before dimension textOmit Specifies diameter/radius symbol is omittedLast Last enum value. Should not be used.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-