DiameterSymbol Enumeration

class NXOpen.Annotations.DiameterSymbol

Bases: object

Specifies the diameter symbol Enum Members

Enum Member Enum Member Description
Dia
Specifies DIA symbol
Standard
Specifies standard symbol
UserDefined
Specifies user defined symbol
Spherical
Specifies spherical symbol
Last
Last enum value. Should not be used.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.