Package | Description |
---|---|
nxopen.weld |
Provides classes and interfaces for Weld.
|
Modifier and Type | Field and Description |
---|---|
static WeldPointReferenceSheetType |
WeldPointReferenceSheetType.NONE
spot welds are points in 3d space
|
static WeldPointReferenceSheetType |
WeldPointReferenceSheetType.OVERLAP
spot welds are based on the intersection of face sets
|
static WeldPointReferenceSheetType |
WeldPointReferenceSheetType.TOP
spot welds are based on the first face set
|
Modifier and Type | Method and Description |
---|---|
WeldPointReferenceSheetType |
WeldPointBuilder.referenceSheetType()
Returns the type of sheet to create to place weld points on.
|
static WeldPointReferenceSheetType |
WeldPointReferenceSheetType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static WeldPointReferenceSheetType |
WeldPointReferenceSheetType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static WeldPointReferenceSheetType[] |
WeldPointReferenceSheetType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
WeldPointBuilder.setReferenceSheetType(WeldPointReferenceSheetType refSheetType)
Sets the type of sheet to create to place weld points on.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.