public class WeldPointReferenceSheetType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_NONE
spot welds are points in 3d space
|
static int |
_OVERLAP
spot welds are based on the intersection of face sets
|
static int |
_TOP
spot welds are based on the first face set
|
static WeldPointReferenceSheetType |
NONE
spot welds are points in 3d space
|
static WeldPointReferenceSheetType |
OVERLAP
spot welds are based on the intersection of face sets
|
static WeldPointReferenceSheetType |
TOP
spot welds are based on the first face set
|
Modifier and Type | Method and Description |
---|---|
static WeldPointReferenceSheetType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static WeldPointReferenceSheetType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static WeldPointReferenceSheetType[] |
values()
Returns an array that contains the values for this enum.
|
public static final WeldPointReferenceSheetType OVERLAP
public static final WeldPointReferenceSheetType TOP
public static final WeldPointReferenceSheetType NONE
public static final int _OVERLAP
public static final int _TOP
public static final int _NONE
public static WeldPointReferenceSheetType valueOf(int value)
public static WeldPointReferenceSheetType valueOf(String name)
public static WeldPointReferenceSheetType[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.