Package | Description |
---|---|
nxopen.validate |
Provides classes and interfaces for Validation Utilities.
|
Modifier and Type | Field and Description |
---|---|
static RequirementCollection.SourceTypeOptions |
RequirementCollection.SourceTypeOptions.LOCAL_FILE |
static RequirementCollection.SourceTypeOptions |
RequirementCollection.SourceTypeOptions.TEAMCENTER |
static RequirementCollection.SourceTypeOptions |
RequirementCollection.SourceTypeOptions.TEAMCENTER_FILE |
Modifier and Type | Method and Description |
---|---|
static RequirementCollection.SourceTypeOptions |
RequirementCollection.SourceTypeOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static RequirementCollection.SourceTypeOptions |
RequirementCollection.SourceTypeOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static RequirementCollection.SourceTypeOptions[] |
RequirementCollection.SourceTypeOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
RequirementCollection.loadFromExternalSource(RequirementCollection.SourceTypeOptions sourceType,
String source,
String revision,
String project)
Loads
Requirement from external source. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.