Package | Description |
---|---|
nxopen.validate |
Provides classes and interfaces for Validation Utilities.
|
Modifier and Type | Field and Description |
---|---|
static RequirementBuilder.RelationalOperatorOptions |
RequirementBuilder.RelationalOperatorOptions.EQUAL |
static RequirementBuilder.RelationalOperatorOptions |
RequirementBuilder.RelationalOperatorOptions.GREATER_THAN |
static RequirementBuilder.RelationalOperatorOptions |
RequirementBuilder.RelationalOperatorOptions.GREATER_THAN_OR_EQUAL |
static RequirementBuilder.RelationalOperatorOptions |
RequirementBuilder.RelationalOperatorOptions.LESS_THAN |
static RequirementBuilder.RelationalOperatorOptions |
RequirementBuilder.RelationalOperatorOptions.LESS_THAN_OR_EQUAL |
static RequirementBuilder.RelationalOperatorOptions |
RequirementBuilder.RelationalOperatorOptions.NOT_EQUAL |
Modifier and Type | Method and Description |
---|---|
RequirementBuilder.RelationalOperatorOptions |
RequirementBuilder.relationalOperatorOption()
Returns the relational operator option between expression label and the value in single sided comparison
License requirements: None. |
RequirementBuilder.RelationalOperatorOptions |
RequirementBuilder.relationalOperatorOptionOnMaximumValue()
Returns the relational operator between expression label and maximum value in double sided comparison:
[expression] < or <= maximum value.
|
RequirementBuilder.RelationalOperatorOptions |
RequirementBuilder.relationalOperatorOptionOnMinimumValue()
Returns the relational operator between minimum value and expression label in double sided comparison:
minimum value < or <= [expression].
|
static RequirementBuilder.RelationalOperatorOptions |
RequirementBuilder.RelationalOperatorOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static RequirementBuilder.RelationalOperatorOptions |
RequirementBuilder.RelationalOperatorOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static RequirementBuilder.RelationalOperatorOptions[] |
RequirementBuilder.RelationalOperatorOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
RequirementBuilder.setRelationalOperatorOption(RequirementBuilder.RelationalOperatorOptions relationalOperatorOption)
License requirements: None. |
void |
RequirementBuilder.setRelationalOperatorOptionOnMaximumValue(RequirementBuilder.RelationalOperatorOptions relationalOperatorOnMaximumValue)
License requirements: None. |
void |
RequirementBuilder.setRelationalOperatorOptionOnMinimumValue(RequirementBuilder.RelationalOperatorOptions relationalOperatorOnMinimumValue)
License requirements: None. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.