Package | Description |
---|---|
nxopen.validate |
Provides classes and interfaces for Validation Utilities.
|
Modifier and Type | Field and Description |
---|---|
static OverrideBuilder.ToStates |
OverrideBuilder.ToStates.FAILED |
static OverrideBuilder.ToStates |
OverrideBuilder.ToStates.PASSED |
Modifier and Type | Method and Description |
---|---|
OverrideBuilder.ToStates |
OverrideBuilder.toState()
Returns the to state of override request
License requirements: None. |
static OverrideBuilder.ToStates |
OverrideBuilder.ToStates.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static OverrideBuilder.ToStates |
OverrideBuilder.ToStates.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static OverrideBuilder.ToStates[] |
OverrideBuilder.ToStates.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
OverrideBuilder.setToState(OverrideBuilder.ToStates toState)
License requirements: ug_checkmate ("UG Check Mate") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.