Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.userdefinedobjects |
Provides classes and interfaces for User Defined Objects (UDOs).
|
Class and Description |
---|
UserDefinedClass
JA interface for the UserDefinedClass object
To create a new instance of this class, use UserDefinedClassManager.newUserDefinedClass() Created in NX5.0.0 |
UserDefinedClassManager
JA interface for the UserDefinedClassManager object
To obtain an instance of this class, refer to Session Created in NX5.0.0 |
UserDefinedObjectManager
This class creates and manages UserDefinedObjects
To obtain an instance of this class, refer to BasePart Created in NX5.0.0 |
Class and Description |
---|
UserDefinedClass
JA interface for the UserDefinedClass object
To create a new instance of this class, use UserDefinedClassManager.newUserDefinedClass() Created in NX5.0.0 |
UserDefinedClass.AllowOwnedObjectSelection
Allow owned object selection on all objects owned by an object of this
UserDefinedClass . |
UserDefinedClass.AllowQueryClass
Allow query class from name options for a
UserDefinedObject of this class. |
UserDefinedClass.DisplayCallback
Prototype for display, selection, attention point, fit and screen-size-fit callbacks
|
UserDefinedClass.GenericCallback
Prototype for information, edit, and suppress callbacks
|
UserDefinedClass.LinkCallback
Prototype for update, and delete callbacks
|
UserDefinedClass.Selection
Allow query class from name options for a
UserDefinedObject . |
UserDefinedDisplayEvent
Implements the Display Event Object for UDO's .
|
UserDefinedEvent
Implements the Event Object for UDO's .
|
UserDefinedEvent.Reason
Available link types for a
UserDefinedObject . |
UserDefinedLinkEvent
Implements the Display Event Object for UDO's .
|
UserDefinedObject
JA interface for the UserDefinedObject object .
|
UserDefinedObject.LinkDefinition
Contains the linked object and it's status along with the type of link.
|
UserDefinedObject.LinkStatus
Status of the object linked to a
nxopen.features.UserDefinedObjectFeature |
UserDefinedObject.LinkType
Available link types for a
nxopen.features.UserDefinedObjectFeature . |
UserDefinedObjectDisplayContext
This class is used to display User Defined Objects .
|
UserDefinedObjectDisplayContext.FacetType
The enumerated type facet to be displayed
|
UserDefinedObjectDisplayContext.PolyMarker
This enumerated type specifies the type of marker to be displayed.
|
UserDefinedObjectDisplayContext.StandardTextRef
This enumerated type specifies the type of reference point used in the text box
for standard_text methods.
|
UserDefinedObjectDisplayContext.TextRef
This enumerated type specifies the type of reference point used in the text box.
|
UserDefinedObjectDisplayContext.TextSize
Provides a way to specify the size of the desired text, as small,
medium or large (normal is a synonym for medium).
|
UserDefinedObjectDisplayContext.ViewMode
The enumerated view mode
|
UserDefinedObjectDisplayContext.ViewModeData
This class holds the data returned from
UserDefinedObjectDisplayContext.getViewMode() |
UserDefinedObjectManager.LinkedUdoDefinition
Used to define a link to a UserDefinedObject
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.