Package | Description |
---|---|
nxopen.userdefinedobjects |
Provides classes and interfaces for User Defined Objects (UDOs).
|
Modifier and Type | Field and Description |
---|---|
static UserDefinedClass.AllowQueryClass |
UserDefinedClass.AllowQueryClass.OFF
You do NOT have permission to query the class from it's name.
|
static UserDefinedClass.AllowQueryClass |
UserDefinedClass.AllowQueryClass.ON
You have permission to query the class from it's name.
|
Modifier and Type | Method and Description |
---|---|
UserDefinedClass.AllowQueryClass |
UserDefinedClass.allowQueryClassFromName()
Returns the allow query class from name flag.
|
static UserDefinedClass.AllowQueryClass |
UserDefinedClass.AllowQueryClass.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static UserDefinedClass.AllowQueryClass |
UserDefinedClass.AllowQueryClass.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static UserDefinedClass.AllowQueryClass[] |
UserDefinedClass.AllowQueryClass.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
UserDefinedClass.setAllowQueryClassFromName(UserDefinedClass.AllowQueryClass allowQueryClassFromName)
Sets the allow query class from name flag.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.