See: Description
Interface | Description |
---|---|
IsvControlPanelBuilder |
Represents a
IsvControlPanelBuilder
To create a new instance of this class, use KinematicConfigurator.createIsvControlPanelBuilder(nxopen.sim.IsvControlPanelBuilder.VisualizationType, nxopen.cam.CAMObject[]) Created in NX8.0.0 |
KinematicAxisBuilder |
Represents the SimKimAxisBuilder class object
Use the KinematicConfigurator class to create a KinematicAxisBuilder object. |
KinematicChain |
This class is used for add kinematic chain to the list.
|
KinematicChainConfiguration |
This class is used for define kinematic chains.
|
KinematicChainList |
Represents a list of objects.
|
KinematicComponent |
Represents the KinematicComponent class object
Use the KinematicConfigurator class to create a KinematicComponent object. |
KinematicComponentBuilder |
Represents the KinamaticComponentBuilder class object
To create a new instance of this class, use KinematicComponentCollection.createHeadBaseComponentBuilder(nxopen.sim.KinematicComponent) Created in NX7.5.0 |
KinematicComponentCollection |
Represents the SimKimComponent Collection
To obtain an instance of this class, refer to KinematicConfigurator Created in NX7.5.0 |
KinematicConfigurator |
Represents the ISV base class object
To obtain an instance of this class, use Part.kinematicConfigurator() Created in NX7.5.0 |
KinematicJunction |
Represents the KinematicJunction class object
Use the KinematicConfigurator class to create a SimKimJunction object. |
KinematicJunctionBuilder |
Represents the SimKimJunctionBuilder class object
Use the KinematicConfigurator class to create a KinematicJunctionBuilder object. |
KinematicJunctionBuilderList |
Represents a list of objects.
|
KinematicSinumerikCaBuilder |
This class is used for edit sinumerik collision avoidance properties.
|
NcChannelSelectionData |
Represents the NcChannelSelectionData class object
Use the NcChannelSelectionData class to create a NcChannelSelectionData object. |
SimDebugBuilder |
Represents a
SimDebugBuilder
To create a new instance of this class, use KinematicConfigurator.createSimDebugBuilder() Created in NX8.0.0 NX_REMOVE_FROM_JAVA_API |
SinumerikCaFacetBuilder |
This class is used for set the facet tolerance.
|
SinumerikCaPlaceholderBuilder |
This class is used for select or unselect component of the placeholder tools.
|
SinumerikCaSimplifyBodiesBuilder |
This class is used for replace geometry.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.