Package | Description |
---|---|
nxopen.routing |
Provides classes and interfaces for Routing.
|
Modifier and Type | Field and Description |
---|---|
static SubdivideSegmentBuilder.EqualSegmentsMethod |
SubdivideSegmentBuilder.EqualSegmentsMethod.EQUAL_ARC_LENGTH
Equal Arc Length
|
static SubdivideSegmentBuilder.EqualSegmentsMethod |
SubdivideSegmentBuilder.EqualSegmentsMethod.EQUAL_PARAMETER
Equal Parameter
|
Modifier and Type | Method and Description |
---|---|
SubdivideSegmentBuilder.EqualSegmentsMethod |
SubdivideSegmentBuilder.equalSegmentsOption()
Returns the equal segments option as
SubdivideSegmentBuilder.EqualSegmentsMethod
License requirements: routing_base ("Routing Basic") Created in NX6.0.0 |
static SubdivideSegmentBuilder.EqualSegmentsMethod |
SubdivideSegmentBuilder.EqualSegmentsMethod.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SubdivideSegmentBuilder.EqualSegmentsMethod |
SubdivideSegmentBuilder.EqualSegmentsMethod.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SubdivideSegmentBuilder.EqualSegmentsMethod[] |
SubdivideSegmentBuilder.EqualSegmentsMethod.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SubdivideSegmentBuilder.setEqualSegmentsOption(SubdivideSegmentBuilder.EqualSegmentsMethod equalSegmentsOption)
License requirements: routing_base ("Routing Basic") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.