Package | Description |
---|---|
nxopen.routing |
Provides classes and interfaces for Routing.
|
Modifier and Type | Field and Description |
---|---|
static RouteManager.BomStockLength |
RouteManager.BomStockLength.LIST_EACH |
static RouteManager.BomStockLength |
RouteManager.BomStockLength.SINGLE_SUM |
Modifier and Type | Method and Description |
---|---|
static RouteManager.BomStockLength |
RouteManager.BomStockLength.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static RouteManager.BomStockLength |
RouteManager.BomStockLength.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static RouteManager.BomStockLength[] |
RouteManager.BomStockLength.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
RouteManager.createBom(RouteManager.BomLevel level,
RouteManager.BomStockLength length,
RouteManager.BomFabrication fabNumbering,
RouteManager.BomBlankLines blankLines,
Part formatFilePart)
Creates Bill of Material (BOM).
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.