Package | Description |
---|---|
nxopen.routing |
Provides classes and interfaces for Routing.
|
Modifier and Type | Field and Description |
---|---|
static ReuseLibrary.ReportInBom |
ReuseLibrary.ReportInBom.DO_NOT_REPORT
Do not report in the Bill of Materials
|
static ReuseLibrary.ReportInBom |
ReuseLibrary.ReportInBom.REPORT
Report in the Bill of Materials
|
Modifier and Type | Method and Description |
---|---|
static ReuseLibrary.ReportInBom |
ReuseLibrary.ReportInBom.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ReuseLibrary.ReportInBom |
ReuseLibrary.ReportInBom.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ReuseLibrary.ReportInBom[] |
ReuseLibrary.ReportInBom.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
RouteManager.createConnectionPostPlacementUdo(ReuseLibrary.PartType udoType,
int numberOfItems,
ReuseLibrary.ReportInBom reportInBOM,
CharacteristicList udoCharx,
PortConnection[] connectionsToLink)
Creates a user defined object (UDO) linked to one or two connections.
|
RouteManager.ModelConnectionPostPlacementGasketData |
RouteManager.modelConnectionPostPlacementGasket(Component placedPart,
PortConnection connection,
ReuseLibrary.ReportInBom reportInBOM,
CharacteristicList gasketCharx)
Places a gasket part based on the gasketCharx
CharacteristicList . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.