Package | Description |
---|---|
nxopen.routing |
Provides classes and interfaces for Routing.
|
Modifier and Type | Field and Description |
---|---|
LineSegment |
SelectLineSegment.ValueData.selection
selected object
|
LineSegment |
SelectLineSegment.ValueWithCaeSetObjectInfoData.selection
selected object
|
LineSegment |
SelectLineSegment.ValueWithSnapData.selection1
first selected object
|
LineSegment |
SelectLineSegment.ValueWithSnapData.selection2
second selected object
|
Modifier and Type | Method and Description |
---|---|
LineSegment |
WindCatcherBuilder.getClosestParentDuctSegment()
Returns the linear segment under the Parent Duct that is closest to the Wind Catcher.
|
LineSegment |
SelectLineSegment.value()
Returns the object being selected
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
EditLineSegmentBuilder |
RouteManager.createEditLineSegmentBuilder(LineSegment line)
Creates a
EditLineSegmentBuilder for editing and locking
the length of line segments. |
void |
EditLineSegmentBuilder.initializeFromLine(LineSegment line)
Initializes (or resets) the builder based off of the input line segment.
|
void |
SelectLineSegment.setValue(LineSegment selection)
Sets the object being selected
License requirements: None. |
void |
SelectLineSegment.setValue(LineSegment selection,
View view,
Point3d point)
The object being selected with the object's view and object's point
License requirements: None. |
void |
SelectLineSegment.setValueWithCaeSetObjectInfo(LineSegment selection,
CaeObjectType.CaeSubType caeSubType,
int caeSubId)
Deprecated.
Deprecated in NX10.0.0. Use other versions of
SelectObject.setValue(nxopen.TaggedObject) .
|
void |
SelectLineSegment.setValueWithSnap(InferSnapType.SnapType snapType,
LineSegment selection1,
View view1,
Point3d point1,
LineSegment selection2,
View view2,
Point3d point2)
The object being selected with the objects view and objects point and snap information.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.