Package | Description |
---|---|
nxopen.routing |
Provides classes and interfaces for Routing.
|
Modifier and Type | Field and Description |
---|---|
static DesignRuleViolationLocationCollection.DeleteOption |
DesignRuleViolationLocationCollection.DeleteOption.DO_DELETE |
static DesignRuleViolationLocationCollection.DeleteOption |
DesignRuleViolationLocationCollection.DeleteOption.DONT_DELETE
Set this option only if you do not want to delete violation location objects
|
Modifier and Type | Method and Description |
---|---|
DesignRuleViolationLocationCollection.DeleteOption |
DesignRuleViolationLocation.deleteLocationObjects()
Returns the function returns delete location objects,
which is an option for deletion of violation location objects.
|
static DesignRuleViolationLocationCollection.DeleteOption |
DesignRuleViolationLocationCollection.DeleteOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DesignRuleViolationLocationCollection.DeleteOption |
DesignRuleViolationLocationCollection.DeleteOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DesignRuleViolationLocationCollection.DeleteOption[] |
DesignRuleViolationLocationCollection.DeleteOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
DesignRuleViolationLocation |
DesignRuleViolationLocationCollection.createDesignRuleViolationLocation(DesignRuleViolationLocationCollection.DeleteOption deleteLocationObjects,
NXObject[] locationObjects)
Creates a
DesignRuleViolationLocation object. |
void |
DesignRuleViolationLocation.setDeleteLocationObjects(DesignRuleViolationLocationCollection.DeleteOption deleteLocationObjects)
Sets the function returns delete location objects,
which is an option for deletion of violation location objects.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.