Package | Description |
---|---|
nxopen.routing |
Provides classes and interfaces for Routing.
|
Modifier and Type | Field and Description |
---|---|
static BranchPathNumberingBuilder.Sequence |
BranchPathNumberingBuilder.Sequence.LOWER_CASE
a, b, c,.....
|
static BranchPathNumberingBuilder.Sequence |
BranchPathNumberingBuilder.Sequence.NUMBERS
1, 2, 3,.....
|
static BranchPathNumberingBuilder.Sequence |
BranchPathNumberingBuilder.Sequence.UPPER_CASE
A, B, C,.....
|
Modifier and Type | Method and Description |
---|---|
BranchPathNumberingBuilder.Sequence |
BranchPathNumberingBuilder.sequenceMethod()
Returns the sequence method specified in the UI for the labels
License requirements: routing_hvac ("Routing HVAC") . |
static BranchPathNumberingBuilder.Sequence |
BranchPathNumberingBuilder.Sequence.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BranchPathNumberingBuilder.Sequence |
BranchPathNumberingBuilder.Sequence.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BranchPathNumberingBuilder.Sequence[] |
BranchPathNumberingBuilder.Sequence.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
BranchPathNumberingBuilder.setSequenceMethod(BranchPathNumberingBuilder.Sequence sequenceMethod)
License requirements: routing_hvac ("Routing HVAC") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.