Package | Description |
---|---|
nxopen.preferences |
Provides classes and interfaces for preferences.
|
Modifier and Type | Field and Description |
---|---|
static SessionVisualizationHighQualityImage.ImageSizeType |
SessionVisualizationHighQualityImage.ImageSizeType.ANSI_A |
static SessionVisualizationHighQualityImage.ImageSizeType |
SessionVisualizationHighQualityImage.ImageSizeType.ANSI_B |
static SessionVisualizationHighQualityImage.ImageSizeType |
SessionVisualizationHighQualityImage.ImageSizeType.ANSI_C |
static SessionVisualizationHighQualityImage.ImageSizeType |
SessionVisualizationHighQualityImage.ImageSizeType.ANSI_D |
static SessionVisualizationHighQualityImage.ImageSizeType |
SessionVisualizationHighQualityImage.ImageSizeType.ANSI_E |
static SessionVisualizationHighQualityImage.ImageSizeType |
SessionVisualizationHighQualityImage.ImageSizeType.FILL_VIEW |
SessionVisualizationHighQualityImage.ImageSizeType |
SessionVisualizationHighQualityImage.ImageSizeData.imageSize |
static SessionVisualizationHighQualityImage.ImageSizeType |
SessionVisualizationHighQualityImage.ImageSizeType.ISO_A0 |
static SessionVisualizationHighQualityImage.ImageSizeType |
SessionVisualizationHighQualityImage.ImageSizeType.ISO_A1 |
static SessionVisualizationHighQualityImage.ImageSizeType |
SessionVisualizationHighQualityImage.ImageSizeType.ISO_A2 |
static SessionVisualizationHighQualityImage.ImageSizeType |
SessionVisualizationHighQualityImage.ImageSizeType.ISO_A3 |
static SessionVisualizationHighQualityImage.ImageSizeType |
SessionVisualizationHighQualityImage.ImageSizeType.ISO_A4 |
static SessionVisualizationHighQualityImage.ImageSizeType |
SessionVisualizationHighQualityImage.ImageSizeType.TRUE_SIZE |
static SessionVisualizationHighQualityImage.ImageSizeType |
SessionVisualizationHighQualityImage.ImageSizeType.USER_DEFINED |
Modifier and Type | Method and Description |
---|---|
static SessionVisualizationHighQualityImage.ImageSizeType |
SessionVisualizationHighQualityImage.ImageSizeType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SessionVisualizationHighQualityImage.ImageSizeType |
SessionVisualizationHighQualityImage.ImageSizeType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SessionVisualizationHighQualityImage.ImageSizeType[] |
SessionVisualizationHighQualityImage.ImageSizeType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SessionVisualizationHighQualityImage.setImageSize(SessionVisualizationHighQualityImage.ImageSizeType imageSize,
int xSize,
int ySize)
Specifies the image size to use for the generation of the High Quality Image.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.