public interface SessionVisualizationHighQualityImage extends Remote
SessionPreferences
Modifier and Type | Interface and Description |
---|---|
static class |
SessionVisualizationHighQualityImage.ImageSizeData
This class holds the data returned from
getImageSize() |
static class |
SessionVisualizationHighQualityImage.ImageSizeType
The size at which to generate a High Quality Image.
|
static class |
SessionVisualizationHighQualityImage.OrientationType
Whether the High Quality Image is to be generated with
portrait or landscape orientation
|
static class |
SessionVisualizationHighQualityImage.PlotQualityType
Describes the quality desired when plotting the High Quality Image
|
static class |
SessionVisualizationHighQualityImage.ResolutionData
This class holds the data returned from
getResolution() |
static class |
SessionVisualizationHighQualityImage.ResolutionType
The resolution to use when generating a High Quality Image.
|
Modifier and Type | Method and Description |
---|---|
SessionVisualizationHighQualityImage.ImageSizeData |
getImageSize()
Returns the image size to use for the generation of the High Quality Image.
|
SessionVisualizationHighQualityImage.ResolutionData |
getResolution()
Returns the resolution to use when generating a High Quality Image.
|
SessionVisualizationHighQualityImage.OrientationType |
orientation()
Returns the orientation for the High Quality Image (portrait or landscape).
|
SessionVisualizationHighQualityImage.PlotQualityType |
plotQuality()
Returns the quality of the plot of the High Quality Image.
|
void |
setImageSize(SessionVisualizationHighQualityImage.ImageSizeType imageSize,
int xSize,
int ySize)
Specifies the image size to use for the generation of the High Quality Image.
|
void |
setOrientation(SessionVisualizationHighQualityImage.OrientationType orientation)
Sets the orientation for the High Quality Image (portrait or landscape).
|
void |
setPlotQuality(SessionVisualizationHighQualityImage.PlotQualityType plotQuality)
Sets the quality of the plot of the High Quality Image.
|
void |
setResolution(SessionVisualizationHighQualityImage.ResolutionType resolution,
int dotsPerInch)
Specifies the resolution to use when generating a High Quality Image.
|
void |
setSubRegion(boolean useSubRegion)
Sets the setting for whether the High Quality Image is generated from a sub-region.
|
boolean |
subRegion()
Returns the setting for whether the High Quality Image is generated from a sub-region.
|
SessionVisualizationHighQualityImage.ImageSizeData getImageSize() throws NXException, RemoteException
NXException
RemoteException
void setImageSize(SessionVisualizationHighQualityImage.ImageSizeType imageSize, int xSize, int ySize) throws NXException, RemoteException
imageSize
- xSize
- X Pixel size. Used only if image_size is user_definedySize
- Y Pixel size. Used only if image_size is user_definedNXException
RemoteException
SessionVisualizationHighQualityImage.OrientationType orientation() throws NXException, RemoteException
NXException
RemoteException
void setOrientation(SessionVisualizationHighQualityImage.OrientationType orientation) throws NXException, RemoteException
orientation
- NXException
RemoteException
SessionVisualizationHighQualityImage.PlotQualityType plotQuality() throws NXException, RemoteException
NXException
RemoteException
void setPlotQuality(SessionVisualizationHighQualityImage.PlotQualityType plotQuality) throws NXException, RemoteException
plotQuality
- NXException
RemoteException
SessionVisualizationHighQualityImage.ResolutionData getResolution() throws NXException, RemoteException
NXException
RemoteException
void setResolution(SessionVisualizationHighQualityImage.ResolutionType resolution, int dotsPerInch) throws NXException, RemoteException
resolution
- dotsPerInch
- Dots per inch.
Used only if resolution is user_definedNXException
RemoteException
boolean subRegion() throws NXException, RemoteException
NXException
RemoteException
void setSubRegion(boolean useSubRegion) throws NXException, RemoteException
useSubRegion
- NXException
RemoteException
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.