Package | Description |
---|---|
nxopen.preferences |
Provides classes and interfaces for preferences.
|
Modifier and Type | Field and Description |
---|---|
static RoutingPath.ChainMethod |
RoutingPath.ChainMethod.CONTINUOUS
Tangents must match at each connection
|
static RoutingPath.ChainMethod |
RoutingPath.ChainMethod.CYCLE
Return all chains
|
static RoutingPath.ChainMethod |
RoutingPath.ChainMethod.MAX_DIST
Chain with maximum path length
|
static RoutingPath.ChainMethod |
RoutingPath.ChainMethod.MIN_DIST
Chain with minimum path length
|
static RoutingPath.ChainMethod |
RoutingPath.ChainMethod.NO_BRANCH
Curves must be mono-connected
|
static RoutingPath.ChainMethod |
RoutingPath.ChainMethod.TANGENT
Use curve with closest tangent when searching
|
Modifier and Type | Method and Description |
---|---|
RoutingPath.ChainMethod |
RoutingPath.getCurveChainingMethod()
Query path curve chaining method
License requirements: routing_base ("Routing Basic") . |
static RoutingPath.ChainMethod |
RoutingPath.ChainMethod.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static RoutingPath.ChainMethod |
RoutingPath.ChainMethod.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static RoutingPath.ChainMethod[] |
RoutingPath.ChainMethod.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
RoutingPath.setCurveChainingMethod(RoutingPath.ChainMethod chainMethod)
License requirements: routing_base ("Routing Basic") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.