public static class RoutingPath.ChainMethod extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CONTINUOUS
Tangents must match at each connection
|
static int |
_CYCLE
Return all chains
|
static int |
_MAX_DIST
Chain with maximum path length
|
static int |
_MIN_DIST
Chain with minimum path length
|
static int |
_NO_BRANCH
Curves must be mono-connected
|
static int |
_TANGENT
Use curve with closest tangent when searching
|
static RoutingPath.ChainMethod |
CONTINUOUS
Tangents must match at each connection
|
static RoutingPath.ChainMethod |
CYCLE
Return all chains
|
static RoutingPath.ChainMethod |
MAX_DIST
Chain with maximum path length
|
static RoutingPath.ChainMethod |
MIN_DIST
Chain with minimum path length
|
static RoutingPath.ChainMethod |
NO_BRANCH
Curves must be mono-connected
|
static RoutingPath.ChainMethod |
TANGENT
Use curve with closest tangent when searching
|
Modifier and Type | Method and Description |
---|---|
static RoutingPath.ChainMethod |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static RoutingPath.ChainMethod |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static RoutingPath.ChainMethod[] |
values()
Returns an array that contains the values for this enum.
|
public static final RoutingPath.ChainMethod NO_BRANCH
public static final RoutingPath.ChainMethod CONTINUOUS
public static final RoutingPath.ChainMethod TANGENT
public static final RoutingPath.ChainMethod CYCLE
public static final RoutingPath.ChainMethod MIN_DIST
public static final RoutingPath.ChainMethod MAX_DIST
public static final int _NO_BRANCH
public static final int _CONTINUOUS
public static final int _TANGENT
public static final int _CYCLE
public static final int _MIN_DIST
public static final int _MAX_DIST
public static RoutingPath.ChainMethod valueOf(int value)
public static RoutingPath.ChainMethod valueOf(String name)
public static RoutingPath.ChainMethod[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.