public interface PartVisualizationEmphasis extends Remote
PartPreferences
Modifier and Type | Interface and Description |
---|---|
static class |
PartVisualizationEmphasis.EdgesType
Determines whether or not edges are displayed for de-emphasized
shaded geometry.
|
static class |
PartVisualizationEmphasis.LayersOptions
Specifies options that control the appearance of de-emphasized
shaded geometry when the See-Thru style is set to Layers.
|
static class |
PartVisualizationEmphasis.OriginalColorShellOptions
Specifies options that control the appearance of de-emphasized
shaded geometry when the See-Thru style is set to Original Color
Shell.
|
static class |
PartVisualizationEmphasis.SeeThruStyleType
Determines how translucency and color are used to de-emphasize
shaded geometry.
|
static class |
PartVisualizationEmphasis.ShellOptions
Specifies options that control the appearance of de-emphasized
shaded geometry when the See-Thru style is set to Shell.
|
static class |
PartVisualizationEmphasis.WireframeBlendOptions
Specifies options that control the color-blending effect used to
de-emphasize wireframe geometry.
|
Modifier and Type | Method and Description |
---|---|
NXColor |
emphasisColor()
Deprecated.
Deprecated in NX9.0.0. This functionality is no longer supported.
|
PartVisualizationEmphasis.LayersOptions |
getLayersOptions()
Returns options that control the appearance of de-emphasized
shaded geometry when the See-Thru style is set to Layers.
|
PartVisualizationEmphasis.OriginalColorShellOptions |
getOriginalColorShellOptions()
Returns options that control the appearance of de-emphasized
shaded geometry when the See-Thru style is set to Original Color
Shell.
|
PartVisualizationEmphasis.ShellOptions |
getShellOptions()
Returns options that control the appearance of de-emphasized
shaded geometry when the See-Thru style is set to Shell.
|
PartVisualizationEmphasis.WireframeBlendOptions |
getWireframeBlendOptions()
Returns options that control the color-blending effect used to
de-emphasize wireframe geometry.
|
PartVisualizationEmphasis.SeeThruStyleType |
seeThruStyle()
Returns the See-Thru style that determines how translucency and color
are used to de-emphasize shaded geometry.
|
void |
setEmphasisColor(NXColor emphasisColor)
Deprecated.
Deprecated in NX9.0.0. This functionality is no longer supported.
|
void |
setLayersOptions(PartVisualizationEmphasis.LayersOptions layersOptions)
Modifies options that control the appearance of de-emphasized
shaded geometry when the See-Thru style is set to Layers.
|
void |
setOriginalColorShellOptions(PartVisualizationEmphasis.OriginalColorShellOptions originalColorShellOptions)
Modifies options that control the appearance of de-emphasized
shaded geometry when the See-Thru style is set to Original Color
Shell.
|
void |
setSeeThruStyle(PartVisualizationEmphasis.SeeThruStyleType seeThruStyle)
Sets the See-Thru style that determines how translucency and color
are used to de-emphasize shaded geometry.
|
void |
setShellOptions(PartVisualizationEmphasis.ShellOptions shellOptions)
Modifies options that control the appearance of de-emphasized
shaded geometry when the See-Thru style is set to Shell.
|
void |
setWireframeBlendOptions(PartVisualizationEmphasis.WireframeBlendOptions wireframeBlendOptions)
Modifies options that control the color-blending effect used to
de-emphasize wireframe geometry.
|
NXColor emphasisColor() throws NXException, RemoteException
NXException
RemoteException
void setEmphasisColor(NXColor emphasisColor) throws NXException, RemoteException
emphasisColor
- NXException
RemoteException
PartVisualizationEmphasis.WireframeBlendOptions getWireframeBlendOptions() throws NXException, RemoteException
NXException
RemoteException
void setWireframeBlendOptions(PartVisualizationEmphasis.WireframeBlendOptions wireframeBlendOptions) throws NXException, RemoteException
wireframeBlendOptions
- options that control the color-blending effect used to
de-emphasize wireframe geometry.NXException
RemoteException
PartVisualizationEmphasis.SeeThruStyleType seeThruStyle() throws NXException, RemoteException
NXException
RemoteException
void setSeeThruStyle(PartVisualizationEmphasis.SeeThruStyleType seeThruStyle) throws NXException, RemoteException
seeThruStyle
- NXException
RemoteException
PartVisualizationEmphasis.ShellOptions getShellOptions() throws NXException, RemoteException
NXException
RemoteException
void setShellOptions(PartVisualizationEmphasis.ShellOptions shellOptions) throws NXException, RemoteException
shellOptions
- options that control the appearance of de-emphasized
shaded geometry when the See-Thru style is set to Shell.NXException
RemoteException
PartVisualizationEmphasis.OriginalColorShellOptions getOriginalColorShellOptions() throws NXException, RemoteException
NXException
RemoteException
void setOriginalColorShellOptions(PartVisualizationEmphasis.OriginalColorShellOptions originalColorShellOptions) throws NXException, RemoteException
originalColorShellOptions
- options that control the appearance of de-emphasized
shaded geometry when the See-Thru style is set to
Original Color Shell.NXException
RemoteException
PartVisualizationEmphasis.LayersOptions getLayersOptions() throws NXException, RemoteException
NXException
RemoteException
void setLayersOptions(PartVisualizationEmphasis.LayersOptions layersOptions) throws NXException, RemoteException
layersOptions
- options that control the appearance of de-emphasized
shaded geometry when the See-Thru style is set to Layers.NXException
RemoteException
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.