public static class PartVisualizationEmphasis.ShellOptions extends Object implements Serializable
Modifier and Type | Field and Description |
---|---|
PartVisualizationEmphasis.EdgesType |
edges
whether or not edges are displayed for de-emphasized
shaded geometry when the See-Thru style is set to Shell.
|
NXColor.Rgb |
edgesRgb
the color of edges displayed for de-emphasized shaded
geometry when the See-Thru style is set to Shell.
|
NXColor.Rgb |
rgb
the color of de-emphasized shaded geometry when the
See-Thru style is set to Shell.
|
int |
translucency
the translucency of de-emphasized shaded geometry when
the See-Thru style is set to Shell.
|
Constructor and Description |
---|
ShellOptions() |
ShellOptions(NXColor.Rgb rgbInitial,
PartVisualizationEmphasis.EdgesType edgesInitial,
NXColor.Rgb edgesRgbInitial,
int translucencyInitial)
Constructor for the ShellOptions object.
|
public NXColor.Rgb rgb
public PartVisualizationEmphasis.EdgesType edges
public NXColor.Rgb edgesRgb
public int translucency
public ShellOptions()
public ShellOptions(NXColor.Rgb rgbInitial, PartVisualizationEmphasis.EdgesType edgesInitial, NXColor.Rgb edgesRgbInitial, int translucencyInitial)
rgbInitial
- the color of de-emphasized shaded geometry when the
See-Thru style is set to Shell.edgesInitial
- whether or not edges are displayed for de-emphasized
shaded geometry when the See-Thru style is set to Shell.edgesRgbInitial
- the color of edges displayed for de-emphasized shaded
geometry when the See-Thru style is set to Shell.translucencyInitial
- the translucency of de-emphasized shaded geometry when
the See-Thru style is set to Shell. It is a percentage
value between 30 and 100.Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.