Package | Description |
---|---|
nxopen.positioning |
Provides classes and interfaces for Assembly Positioning and Constraints.
|
Modifier and Type | Field and Description |
---|---|
static Constraint.Alignment |
Constraint.Alignment.CO_ALIGN
Directions are the same
|
static Constraint.Alignment |
Constraint.Alignment.CONTRA_ALIGN
Directions are opposite
|
static Constraint.Alignment |
Constraint.Alignment.INFER_ALIGN
Allow the solver to decide the alignment
|
Modifier and Type | Method and Description |
---|---|
Constraint.Alignment |
Constraint.constraintAlignment()
Returns
the alignment behavior for the constraint.
|
static Constraint.Alignment |
Constraint.Alignment.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Constraint.Alignment |
Constraint.Alignment.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Constraint.Alignment[] |
Constraint.Alignment.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
Constraint.setAlignmentHint(Constraint.Alignment alignment)
Set a hint as to which alignment should be used by the
solver for this constraint.
|
void |
Constraint.setConstraintAlignment(Constraint.Alignment alignment)
License requirements: assemblies ("ASSEMBLIES MODULE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.