See: Description
Interface | Description |
---|---|
ComponentConstraint |
Constraint for use in positioning assembly objects in NX.
|
ComponentNetwork |
Network for use in positioning components in NX.
|
ComponentPositioner |
An instance of this class can be used to create
Constraint s and
associated objects. |
Constraint |
Constraint for use in positioning objects in NX.
|
ConstraintCollection |
a collection of constraints
To obtain an instance of this class, refer to Positioner Created in NX5.0.0 |
ConstraintReference |
ConstraintReference for use in positioning objects in NX.
|
DisplayedConstraint |
The displayed representation of a constraint, used for graphical
display and to represent it in the Assembly Navigator.
|
DisplayedConstraintCollection |
a collection of displayed constraints
To obtain an instance of this class, refer to Part Created in NX7.5.0 |
MatingConverter |
An instance of this class can be used to convert Mating Conditions
to Assembly Constraints in its owning assembly or in child parts
of its owning assembly.
|
Network |
Network for use in positioning objects in NX.
|
Positioner |
An instance of this class can be used to create
Constraint s and
associated objects. |
Class | Description |
---|---|
ComponentConstraint.DirectionToFixed |
Specifies how a constraint affects the positioning of a component.
|
ComponentNetwork.ArrangementsMode |
Specifies how changes in the network are applied to arrangements.
|
Constraint.Alignment |
Specifies alignment of directed geometries used in a constraint.
|
Constraint.SolverStatus |
Specifies the status of a constraint.
|
Constraint.SplineType |
Specifies how the spline points define the shape of the spline.
|
Constraint.Type |
Specifies the type of a constraint.
|
ConstraintReference.ConstraintOrder |
Specifies the order of the constraint reference used in a
Constraint . |
ConstraintReference.GeometryType |
Specifies the type of the geometry used in a
ConstraintReference . |
ConstraintReference.HalfSpace |
Specifies the half space value of one geometry used in a distance constraint.
|
MatingConverter.PartContext |
Defines in which parts mating conditions will be converted.
|
Network.ObjectStatus |
Specifies the solver status of a movable object.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.