Package | Description |
---|---|
nxopen.positioning |
Provides classes and interfaces for Assembly Positioning and Constraints.
|
Modifier and Type | Field and Description |
---|---|
static ComponentNetwork.ArrangementsMode |
ComponentNetwork.ArrangementsMode.EXISTING
Apply transforms in arrangements according to existing component properties.
|
static ComponentNetwork.ArrangementsMode |
ComponentNetwork.ArrangementsMode.IN_USED
Apply transforms in the used arrangement only.
|
Modifier and Type | Method and Description |
---|---|
ComponentNetwork.ArrangementsMode |
ComponentNetwork.networkArrangementsMode()
Returns
the arrangements mode for this network.
|
static ComponentNetwork.ArrangementsMode |
ComponentNetwork.ArrangementsMode.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ComponentNetwork.ArrangementsMode |
ComponentNetwork.ArrangementsMode.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ComponentNetwork.ArrangementsMode[] |
ComponentNetwork.ArrangementsMode.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ComponentNetwork.setNetworkArrangementsMode(ComponentNetwork.ArrangementsMode mode)
License requirements: assemblies ("ASSEMBLIES MODULE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.