Package | Description |
---|---|
nxopen.pdm |
Provides classes and interfaces for PDM.
|
Modifier and Type | Field and Description |
---|---|
static CaeCloneManager.CloneOption |
CaeCloneManager.CloneOption.FEM |
static CaeCloneManager.CloneOption |
CaeCloneManager.CloneOption.IDEAL |
static CaeCloneManager.CloneOption |
CaeCloneManager.CloneOption.MASTER |
static CaeCloneManager.CloneOption |
CaeCloneManager.CloneOption.NONE |
static CaeCloneManager.CloneOption |
CaeCloneManager.CloneOption.SIM |
Modifier and Type | Method and Description |
---|---|
static CaeCloneManager.CloneOption |
CaeCloneManager.CloneOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CaeCloneManager.CloneOption |
CaeCloneManager.CloneOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CaeCloneManager.CloneOption[] |
CaeCloneManager.CloneOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
String |
CaeCloneManager.getContainer(CaeCloneManager.CloneOption option)
Deprecated.
Deprecated in NX10.0.0. Use
PartOperationCopyBuilder instead.
|
PartFromPartBuilder |
CaeCloneManager.getPartBuilderForClone(CaeCloneManager.CloneOption option)
Deprecated.
Deprecated in NX10.0.0. Use
PartOperationCopyBuilder instead.
|
void |
CaeCloneManager.setContainer(CaeCloneManager.CloneOption option,
String container)
Deprecated.
Deprecated in NX10.0.0. Use
PartOperationCopyBuilder instead.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.