Modifier and Type | Method and Description |
---|---|
void |
createTraceLinks(String[] requirementItemNumbers,
String[] requirementRevisions,
String[] parts)
Creates Trace Links from
Requirement s to Part s
For the input requirement_item_numbers:
In case of Default Domain: it is Teamcenter item ID. |
TracelinkQuery |
newTracelinkQuery()
Returns a Tracelink query object
License requirements: None. |
void |
removeTraceLinks(String[] requirementItemNumbers,
String[] requirementRevisions,
String[] parts)
Removes Trace Links between
Requirement s and Part s
For the input requirement_item_numbers:
In case of Default Domain: it is Teamcenter item ID. |
TracelinkQuery newTracelinkQuery() throws NXException, RemoteException
NXException
RemoteException
void createTraceLinks(String[] requirementItemNumbers, String[] requirementRevisions, String[] parts) throws NXException, RemoteException
Requirement
s to Part
s
For the input requirement_item_numbers:
In case of Default Domain: it is Teamcenter item ID.
In case of non-Default Domain: it is the multifield key.
e.g. %#MFK#%,=item_id=001, object_type=SupplierPart, supplier_code=x
And the encoded part filename would be containing the MFK.
requirementItemNumbers
- requirement multifield keyrequirementRevisions
- requirement item revisions. Must be same size as the item number arrayparts
- part CLI names NXException
RemoteException
void removeTraceLinks(String[] requirementItemNumbers, String[] requirementRevisions, String[] parts) throws NXException, RemoteException
Requirement
s and Part
s
For the input requirement_item_numbers:
In case of Default Domain: it is Teamcenter item ID.
In case of non-Default Domain: it is the multifield key.
e.g. %#MFK#%,=item_id=001, object_type=SupplierPart, supplier_code=x
And the encoded part filename would be containing the MFK.
requirementItemNumbers
- requirement multifield KeyrequirementRevisions
- requirement item revisions. Must be same size as the item number arrayparts
- part CLI names NXException
RemoteException
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.