Package | Description |
---|---|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Field and Description |
---|---|
static ShapeFrameBuilder.AnchorAttachmentType |
ShapeFrameBuilder.AnchorAttachmentType.CENTER
Anchor is attached to the center of the frame
|
static ShapeFrameBuilder.AnchorAttachmentType |
ShapeFrameBuilder.AnchorAttachmentType.NONE
Anchor is not attached to the frame
|
static ShapeFrameBuilder.AnchorAttachmentType |
ShapeFrameBuilder.AnchorAttachmentType.VERTEX1
Anchor is attached to the first vertex of the frame
|
static ShapeFrameBuilder.AnchorAttachmentType |
ShapeFrameBuilder.AnchorAttachmentType.VERTEX2
Anchor is attached to the second vertex of the frame
|
static ShapeFrameBuilder.AnchorAttachmentType |
ShapeFrameBuilder.AnchorAttachmentType.VERTEX3
Anchor is attached to the third vertex of the frame
|
static ShapeFrameBuilder.AnchorAttachmentType |
ShapeFrameBuilder.AnchorAttachmentType.VERTEX4
Anchor is attached to the fourth vertex of the frame
|
Modifier and Type | Method and Description |
---|---|
ShapeFrameBuilder.AnchorAttachmentType |
ShapeFrameBuilder.anchorAttachment()
Returns the anchor attachment
License requirements: None. |
static ShapeFrameBuilder.AnchorAttachmentType |
ShapeFrameBuilder.AnchorAttachmentType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ShapeFrameBuilder.AnchorAttachmentType |
ShapeFrameBuilder.AnchorAttachmentType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ShapeFrameBuilder.AnchorAttachmentType[] |
ShapeFrameBuilder.AnchorAttachmentType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ShapeFrameBuilder.setAnchorAttachment(ShapeFrameBuilder.AnchorAttachmentType anchorAttachment)
License requirements: None. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.