public static class ShapeFrameBuilder.AnchorAttachmentType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CENTER
Anchor is attached to the center of the frame
|
static int |
_NONE
Anchor is not attached to the frame
|
static int |
_VERTEX1
Anchor is attached to the first vertex of the frame
|
static int |
_VERTEX2
Anchor is attached to the second vertex of the frame
|
static int |
_VERTEX3
Anchor is attached to the third vertex of the frame
|
static int |
_VERTEX4
Anchor is attached to the fourth vertex of the frame
|
static ShapeFrameBuilder.AnchorAttachmentType |
CENTER
Anchor is attached to the center of the frame
|
static ShapeFrameBuilder.AnchorAttachmentType |
NONE
Anchor is not attached to the frame
|
static ShapeFrameBuilder.AnchorAttachmentType |
VERTEX1
Anchor is attached to the first vertex of the frame
|
static ShapeFrameBuilder.AnchorAttachmentType |
VERTEX2
Anchor is attached to the second vertex of the frame
|
static ShapeFrameBuilder.AnchorAttachmentType |
VERTEX3
Anchor is attached to the third vertex of the frame
|
static ShapeFrameBuilder.AnchorAttachmentType |
VERTEX4
Anchor is attached to the fourth vertex of the frame
|
Modifier and Type | Method and Description |
---|---|
static ShapeFrameBuilder.AnchorAttachmentType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ShapeFrameBuilder.AnchorAttachmentType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ShapeFrameBuilder.AnchorAttachmentType[] |
values()
Returns an array that contains the values for this enum.
|
public static final ShapeFrameBuilder.AnchorAttachmentType NONE
public static final ShapeFrameBuilder.AnchorAttachmentType CENTER
public static final ShapeFrameBuilder.AnchorAttachmentType VERTEX1
public static final ShapeFrameBuilder.AnchorAttachmentType VERTEX2
public static final ShapeFrameBuilder.AnchorAttachmentType VERTEX3
public static final ShapeFrameBuilder.AnchorAttachmentType VERTEX4
public static final int _NONE
public static final int _CENTER
public static final int _VERTEX1
public static final int _VERTEX2
public static final int _VERTEX3
public static final int _VERTEX4
public static ShapeFrameBuilder.AnchorAttachmentType valueOf(int value)
public static ShapeFrameBuilder.AnchorAttachmentType valueOf(String name)
public static ShapeFrameBuilder.AnchorAttachmentType[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.