Package | Description |
---|---|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Field and Description |
---|---|
static Rebuild.RebuildTypes |
Rebuild.RebuildTypes.ADVANCED
Specify the maximum degree and maximum segments to rebuild.
|
static Rebuild.RebuildTypes |
Rebuild.RebuildTypes.KEEP_PARAMETERIZATION
Keep the parameterization
|
static Rebuild.RebuildTypes |
Rebuild.RebuildTypes.MANUAL
Specify the rebuild degree manually.
|
static Rebuild.RebuildTypes |
Rebuild.RebuildTypes.NONE
No degree entry or simple integer/enumerable value used to specify the rebuild degree.
|
Modifier and Type | Method and Description |
---|---|
Rebuild.RebuildTypes |
Rebuild.rebuildType()
Returns the rebuild type.
|
static Rebuild.RebuildTypes |
Rebuild.RebuildTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Rebuild.RebuildTypes |
Rebuild.RebuildTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Rebuild.RebuildTypes[] |
Rebuild.RebuildTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
Rebuild.setRebuildType(Rebuild.RebuildTypes rebuildType)
Sets the rebuild type.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.