public static class Rebuild.RebuildTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ADVANCED
Specify the maximum degree and maximum segments to rebuild.
|
static int |
_KEEP_PARAMETERIZATION
Keep the parameterization
|
static int |
_MANUAL
Specify the rebuild degree manually.
|
static int |
_NONE
No degree entry or simple integer/enumerable value used to specify the rebuild degree.
|
static Rebuild.RebuildTypes |
ADVANCED
Specify the maximum degree and maximum segments to rebuild.
|
static Rebuild.RebuildTypes |
KEEP_PARAMETERIZATION
Keep the parameterization
|
static Rebuild.RebuildTypes |
MANUAL
Specify the rebuild degree manually.
|
static Rebuild.RebuildTypes |
NONE
No degree entry or simple integer/enumerable value used to specify the rebuild degree.
|
Modifier and Type | Method and Description |
---|---|
static Rebuild.RebuildTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Rebuild.RebuildTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Rebuild.RebuildTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final Rebuild.RebuildTypes NONE
public static final Rebuild.RebuildTypes MANUAL
public static final Rebuild.RebuildTypes ADVANCED
public static final Rebuild.RebuildTypes KEEP_PARAMETERIZATION
public static final int _NONE
public static final int _MANUAL
public static final int _ADVANCED
public static final int _KEEP_PARAMETERIZATION
public static Rebuild.RebuildTypes valueOf(int value)
public static Rebuild.RebuildTypes valueOf(String name)
public static Rebuild.RebuildTypes[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.