Package | Description |
---|---|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Field and Description |
---|---|
static OnPathDimensionBuilder.UpdateReason |
OnPathDimensionBuilder.UpdateReason.ALL
Update because either path or through point location may have changed
|
static OnPathDimensionBuilder.UpdateReason |
OnPathDimensionBuilder.UpdateReason.PATH
Update because of the path may have changed
|
static OnPathDimensionBuilder.UpdateReason |
OnPathDimensionBuilder.UpdateReason.THROUGH_POINT
Update because the through point location may have changed
|
Modifier and Type | Method and Description |
---|---|
static OnPathDimensionBuilder.UpdateReason |
OnPathDimensionBuilder.UpdateReason.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static OnPathDimensionBuilder.UpdateReason |
OnPathDimensionBuilder.UpdateReason.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static OnPathDimensionBuilder.UpdateReason[] |
OnPathDimensionBuilder.UpdateReason.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
OnPathDimensionBuilder.update(OnPathDimensionBuilder.UpdateReason updateReason)
Updates this object if the path or through point location has changed.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.