public static class OnPathDimensionBuilder.UpdateReason extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ALL
Update because either path or through point location may have changed
|
static int |
_PATH
Update because of the path may have changed
|
static int |
_THROUGH_POINT
Update because the through point location may have changed
|
static OnPathDimensionBuilder.UpdateReason |
ALL
Update because either path or through point location may have changed
|
static OnPathDimensionBuilder.UpdateReason |
PATH
Update because of the path may have changed
|
static OnPathDimensionBuilder.UpdateReason |
THROUGH_POINT
Update because the through point location may have changed
|
Modifier and Type | Method and Description |
---|---|
static OnPathDimensionBuilder.UpdateReason |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static OnPathDimensionBuilder.UpdateReason |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static OnPathDimensionBuilder.UpdateReason[] |
values()
Returns an array that contains the values for this enum.
|
public static final OnPathDimensionBuilder.UpdateReason PATH
public static final OnPathDimensionBuilder.UpdateReason THROUGH_POINT
public static final OnPathDimensionBuilder.UpdateReason ALL
public static final int _PATH
public static final int _THROUGH_POINT
public static final int _ALL
public static OnPathDimensionBuilder.UpdateReason valueOf(int value)
public static OnPathDimensionBuilder.UpdateReason valueOf(String name)
public static OnPathDimensionBuilder.UpdateReason[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.