Package | Description |
---|---|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Field and Description |
---|---|
static EndHoleData.ThreadRotationOptions |
EndHoleData.ThreadRotationOptions.LEFT
Left rotation
|
static EndHoleData.ThreadRotationOptions |
EndHoleData.ThreadRotationOptions.RIGHT
Right rotation
|
Modifier and Type | Method and Description |
---|---|
EndHoleData.ThreadRotationOptions |
EndHoleData.threadRotation()
Returns the thread rotation
License requirements: None. |
static EndHoleData.ThreadRotationOptions |
EndHoleData.ThreadRotationOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static EndHoleData.ThreadRotationOptions |
EndHoleData.ThreadRotationOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static EndHoleData.ThreadRotationOptions[] |
EndHoleData.ThreadRotationOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
EndHoleData.setThreadRotation(EndHoleData.ThreadRotationOptions threadRotation)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.