Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.features |
Provides classes and interfaces for features.
|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Method and Description |
---|---|
BlendSetbackBuilder |
Part.createEmptyBlendSetbackBuilder()
Creates a
BlendSetbackBuilder object
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
BlendSetbackBuilder |
BlendCornerBuilder.createBlendSetbackBuilder()
Create a blend setback builder object.
|
Modifier and Type | Method and Description |
---|---|
BlendSetbackBuilder |
BlendSetbackBuilderList.findItem(int index)
Returns the object at the input index.
|
BlendSetbackBuilder[] |
BlendSetbackBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
BlendSetbackBuilderList.append(BlendSetbackBuilder object)
Appends an object to the list
License requirements: None. |
void |
BlendSetbackBuilderList.append(BlendSetbackBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
BlendSetbackBuilderList.erase(BlendSetbackBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
BlendSetbackBuilderList.erase(BlendSetbackBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
BlendSetbackBuilderList.findIndex(BlendSetbackBuilder obj)
Finds the index where the input object appears.
|
void |
BlendSetbackBuilderList.insert(int location,
BlendSetbackBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
BlendSetbackBuilderList.setContents(BlendSetbackBuilder[] objects)
Sets the contents of the entire list.
|
void |
BlendSetbackBuilderList.swap(BlendSetbackBuilder object1,
BlendSetbackBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.