Package | Description |
---|---|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Field and Description |
---|---|
static AlongPathPattern.YDirectionOptions |
AlongPathPattern.YDirectionOptions.SECTION
y direction is a section.
|
static AlongPathPattern.YDirectionOptions |
AlongPathPattern.YDirectionOptions.VECTOR
y direction is a vector.
|
Modifier and Type | Method and Description |
---|---|
static AlongPathPattern.YDirectionOptions |
AlongPathPattern.YDirectionOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AlongPathPattern.YDirectionOptions |
AlongPathPattern.YDirectionOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AlongPathPattern.YDirectionOptions[] |
AlongPathPattern.YDirectionOptions.values()
Returns an array that contains the values for this enum.
|
AlongPathPattern.YDirectionOptions |
AlongPathPattern.ydirectionOption()
Returns the y direction options
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
AlongPathPattern.setYDirectionOption(AlongPathPattern.YDirectionOptions yDirectionOption)
License requirements: None. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.