public static class AlongPathPattern.YDirectionOptions extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_SECTION
y direction is a section.
|
static int |
_VECTOR
y direction is a vector.
|
static AlongPathPattern.YDirectionOptions |
SECTION
y direction is a section.
|
static AlongPathPattern.YDirectionOptions |
VECTOR
y direction is a vector.
|
Modifier and Type | Method and Description |
---|---|
static AlongPathPattern.YDirectionOptions |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AlongPathPattern.YDirectionOptions |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AlongPathPattern.YDirectionOptions[] |
values()
Returns an array that contains the values for this enum.
|
public static final AlongPathPattern.YDirectionOptions VECTOR
public static final AlongPathPattern.YDirectionOptions SECTION
public static final int _VECTOR
public static final int _SECTION
public static AlongPathPattern.YDirectionOptions valueOf(int value)
public static AlongPathPattern.YDirectionOptions valueOf(String name)
public static AlongPathPattern.YDirectionOptions[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.