Package | Description |
---|---|
nxopen.geometricanalysis |
Provides classes and interfaces for Geometric Analysis.
|
Modifier and Type | Field and Description |
---|---|
static HighlightLinesAnalysisBuilder.DisplayMethods |
HighlightLinesAnalysisBuilder.DisplayMethods.PROJECTION
Deprecated.
Create projection lines
|
static HighlightLinesAnalysisBuilder.DisplayMethods |
HighlightLinesAnalysisBuilder.DisplayMethods.REFLECTION
Deprecated.
Create reflection lines
|
Modifier and Type | Method and Description |
---|---|
HighlightLinesAnalysisBuilder.DisplayMethods |
HighlightLinesAnalysisBuilder.displayMethod()
Deprecated.
Deprecated in NX8.0.0. Use
HighlightLinesAnalysisBuilder.type2() and HighlightLinesAnalysisBuilder.setType2(nxopen.geometricanalysis.HighlightLinesAnalysisBuilder.Types2) instead.
|
static HighlightLinesAnalysisBuilder.DisplayMethods |
HighlightLinesAnalysisBuilder.DisplayMethods.valueOf(int value)
Deprecated.
Returns the enum constant of the specified enum type with the specified value.
|
static HighlightLinesAnalysisBuilder.DisplayMethods |
HighlightLinesAnalysisBuilder.DisplayMethods.valueOf(String name)
Deprecated.
Returns the enum constant of the specified enum type with the specified name.
|
static HighlightLinesAnalysisBuilder.DisplayMethods[] |
HighlightLinesAnalysisBuilder.DisplayMethods.values()
Deprecated.
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
HighlightLinesAnalysisBuilder.setDisplayMethod(HighlightLinesAnalysisBuilder.DisplayMethods displayMethod)
Deprecated.
Deprecated in NX8.0.0. Use
HighlightLinesAnalysisBuilder.type2() and HighlightLinesAnalysisBuilder.setType2(nxopen.geometricanalysis.HighlightLinesAnalysisBuilder.Types2) instead.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.