Package | Description |
---|---|
nxopen.geometricanalysis |
Provides classes and interfaces for Geometric Analysis.
|
Modifier and Type | Field and Description |
---|---|
static GapFlushnessBuilder.SectionCurveOptions |
GapFlushnessBuilder.SectionCurveOptions.CONTACT_CURVE
use contact curve
|
static GapFlushnessBuilder.SectionCurveOptions |
GapFlushnessBuilder.SectionCurveOptions.USER_DEFINED
use user defined curve
|
Modifier and Type | Method and Description |
---|---|
GapFlushnessBuilder.SectionCurveOptions |
GapFlushnessBuilder.crossSectionCurveOption()
Returns the cross section curve option
License requirements: solid_modeling ("SOLIDS MODELING") . |
static GapFlushnessBuilder.SectionCurveOptions |
GapFlushnessBuilder.SectionCurveOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static GapFlushnessBuilder.SectionCurveOptions |
GapFlushnessBuilder.SectionCurveOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static GapFlushnessBuilder.SectionCurveOptions[] |
GapFlushnessBuilder.SectionCurveOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
GapFlushnessBuilder.setCrossSectionCurveOption(GapFlushnessBuilder.SectionCurveOptions sectionCurveOption)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.