public static class FieldEvaluator.ValuesOutsideTableInterpolationEnum extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CONSTANT
Returns the boundary value as interpolation result
|
static int |
_EXTRAPOLATE
Extrapolates from the boundary out into space using the same interpolation method that the interpolator for interior table values uses
|
static int |
_UNDEFINED
No interpolation result
|
static FieldEvaluator.ValuesOutsideTableInterpolationEnum |
CONSTANT
Returns the boundary value as interpolation result
|
static FieldEvaluator.ValuesOutsideTableInterpolationEnum |
EXTRAPOLATE
Extrapolates from the boundary out into space using the same interpolation method that the interpolator for interior table values uses
|
static FieldEvaluator.ValuesOutsideTableInterpolationEnum |
UNDEFINED
No interpolation result
|
Modifier and Type | Method and Description |
---|---|
static FieldEvaluator.ValuesOutsideTableInterpolationEnum |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FieldEvaluator.ValuesOutsideTableInterpolationEnum |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FieldEvaluator.ValuesOutsideTableInterpolationEnum[] |
values()
Returns an array that contains the values for this enum.
|
public static final FieldEvaluator.ValuesOutsideTableInterpolationEnum UNDEFINED
public static final FieldEvaluator.ValuesOutsideTableInterpolationEnum EXTRAPOLATE
public static final FieldEvaluator.ValuesOutsideTableInterpolationEnum CONSTANT
public static final int _UNDEFINED
public static final int _EXTRAPOLATE
public static final int _CONSTANT
public static FieldEvaluator.ValuesOutsideTableInterpolationEnum valueOf(int value)
public static FieldEvaluator.ValuesOutsideTableInterpolationEnum valueOf(String name)
public static FieldEvaluator.ValuesOutsideTableInterpolationEnum[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.